Hi,
I was successfull boot kernel by uboot2016 and boot uboot by spl on the IMX6DQ . But i can't boot kernel directy by spl.
The log is stopped at: Uncompressing Linux... done, booting the kernel.
I have set up boot parameters and machine code in SPL.
Can you give me some suggestions?
Thanks.
Hi zero
one can try to test memory and update ddr initialization
with new calibration settings found from test
i.MX6/7 DDR Stress Test Tool V2.92
may be useful to check spl tutorial :
ventana/bootloader – Gateworks
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
The SPL can start uboot ,then starts kernel is successful. The DDR parameters used by SPL and UBOOT should be the same set.
If DDR parameter is a problem, uboot should start kernel failure. Or is there any other reason? (I was use uboot 2016 boot kernel 3.0.35)
Thanks..