Hello all,
Im trying to set up a device tree for some custom hardware and had a mux question regarding SPI.
Ive looked at the imx6qdl-nitrogen6_max.dtsi as part of the boundary 3.14 linux release. The spi chipselects in the nitrogen and sabre boards are all tied to GPIO's however our spi CS isnt done using gpio. For example Spi 1's ss0 is on pin disp0_data23.
The current device tree sets spi CS up as:
fsl,spi-num-chiselects = <1> (this should be ok for ours as well)
cs-gpios = GP_ECSPI1_NOR_CS
where
GP_ECSPI1_NOR_CS is a #define pointing to a gpio bank and pin.
If were using the disp0 line for the ss0 do i just define it as:
MX6QDL_PAD_DISP0_DAT23_ECSPI1_SSO 0x100b1
following the same pattern as the other muxes and get rid of the cs-gpios = ... line or is it done differently?
Hi matthew
according documentation and probe function in linux/drivers/spi/spi-imx.c
linux-2.6-imx.git - Freescale i.MX Linux Tree
linux-2.6-imx.git - Freescale i.MX Linux Tree
seems implemented only option with "cs-gpios".
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------