SPI 5 not working on IMX6QP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI 5 not working on IMX6QP

701件の閲覧回数
michal_olbrich
Contributor I

Hello,

I am writing my own SPI driver. I need to use ECSPI 5 on iMX6QP. I am following the instructions in the datasheet regarding the initialization of the the ECSPI 5 module. I am configuring the registers directly using /dev/mem and mmap funtion.

The problem is, I am not able to measure any CLK singal on the pad SD1_CLK.

The instructions in the Datasheet are:

    1. Clear the EN bit in ECSPI_CONREG to reset the block.
    2. Enable the clocks for ECSPI within the CCM.
    3. Configure the Control Register and then set the EN bit in the ECSPI_CONREG to
    put ECSPI out of reset.
    4. Configure corresponding IOMUX for ECSPI external signals.
    5. Configure registers of ECSPI properly according to the specifications of the external


I do everything listed above. I suspect, that there is a problem with the CCM. There is a register CCM Clock Gating Register 1 (CCM_CCGR1) where I enable the CG4 ecspi5 clocks (ecspi5_clk_enable). But I am not sure about other registers in CCM.

According to the Table 18-3. System Clocks, Gating, and Override, this field should enable signals ipg_clk and ipg_clk_per.

But there is also CCM Clock Output Source Register (CCM_CCOSR), there is field CLKO2_SEL where I set ecspi_clk_root and also CLKO2_EN which I enable.


IO-MUX setting:

IOMUXC_ECSPI5_CSPI_CLK_IN_SELECT_INPUT is set to 0: SD1_CLK_ALT1

(with ALT2 — Select signal XTALOSC_OSC32K_32K_OUT I can see clk signal, so the PAD is ok)

IOMUXC_SW_MUX_CTL_PAD_SD1_CLK is set to 001: ALT1 — Select signal ECSPI5_SCLK.

Control Register (ECSPI5_CONREG) is in the end set to: 0x000458F1

CHANNEL_SELECT: 01b

PRE_DIVIDER: 101b (6x)

POST_DIVIDER: 1000b (256x)

CHANNEL_MODE: 1111b

I also tried to modify the devicetree:

ecspi@02018000 {
                    #address-cells = <0x1>;
                    #size-cells = <0x0>;
                    compatible = "fsl,imx6q-ecspi", "fsl,imx51-ecspi";
                    reg = <0x2018000 0x4000>;
                    interrupts = <0x0 0x23 0x4>;
                    clocks = <0x2 0x74 0x2 0x74>;
                    clock-names = "ipg", "per";
                    dmas = <0xe 0xb 0x8 0x1 0xe 0xc 0x8 0x2>;
                    dma-names = "rx", "tx";
                    status = "ok";
                    spidev@0 {
                        compatible = "spidev";
                        spi-max-frequency = <20000000>;
                        reg = <0>;
                        };
                };

I am able to see then the  /dev/spidev4.0 . This sets the ECSPI5_CONREG to 0x0070E3F1, which is a valid setting, but an spi example test program, which uses dev/spidev fails and I am neither able to see clk signal on the associated PAD. (I modify the IOMUX by mmap in this case as well).

Please help.

ラベル(1)
タグ(2)
0 件の賞賛
1 返信

624件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Michal

for ecspi initialization sequence may be useful to check baremetal sdk example

rt-thread/bsp/imx6sx/iMX6_Platform_SDK/sdk/drivers/spi/src at master · RT-Thread/rt-thread · GitHub 

spidev description:

Enabling SPI on DART-MX6 [SOLVED] - Variscite Forums 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛