I have some questions about SLN-VIZNAS-IOT.
1.How should I demo SLN-VIZNAS-IOT PDM MEMS Microphones?
2.Does i.MX RT106F have the same microphone function as i.MX RT1060?
i.MX RT106F use PDM MEMS Microphones but the SDK (SDK_2_8_1_SLN-VIZNAS-IOT) seems no audio output about PDM MEMS Microphones.
Please help me to solve these problem. Thanks
已解决! 转到解答。
So for SLN-VIZNAS-IOT, Will the SDK be updated about PDM MEMS Microphones in the future?
The SDK_2_8_1_SLN-VIZNAS-IOT seems no PDM mic Init , so the SDK_2_8_1_SLN-VIZNAS-IOT can
not use PDM MEMS Microphones?
Please give me the answer. Thanks
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1. How should I demo SLN-VIZNAS-IOT PDM MEMS Microphones?
-- For SLN-VIZNAS-IOT, the SDK library hasn't such a demo to test the Microphones on the board until now.
2. Does i.MX RT106F have the same microphone function as i.MX RT1060?
-- Yes.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
So for SLN-VIZNAS-IOT, Will the SDK be updated about PDM MEMS Microphones in the future?
The SDK_2_8_1_SLN-VIZNAS-IOT seems no PDM mic Init , so the SDK_2_8_1_SLN-VIZNAS-IOT can
not use PDM MEMS Microphones?
Please give me the answer. Thanks
Hi,
Thanks for your reply.
1) So for SLN-VIZNAS-IOT, Will the SDK be updated about PDM MEMS Microphones in the future?
-- To be honest, I don't know and I guess they don't have the plan currently.
Hope it helps.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Thanks for your reply.
1) So any suggestions about developing PDM MIC on the SLN-VIZNAS-IOT? Or I can refer to which SDK?
-- Please refer to the interrupt_record_playback demo in the SDK library for MIMXRT1060-EVK.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
I study about interrupt_record_playback demo in the SDK library for MIMXRT1060-EVK. But it doesn't seem to use PDM mircophone. This demo uses both headphone mic and board main mic as input source.So it seems a little different ? So any suggestions about developing PDM MIC on the SLN-VIZNAS-IOT ? Or where can I start ? Thanks
Hi,
Thanks for your reply.
Please refer to the driver in the SDK library for SLN-LOCAL2-IOT which uses SPH0641LM4H too.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank you for your reply.
I referred to your suggestion SDK library for SLN-LOCAL2-IOT.
I see that I can do this individually with SAI1, SAI2, and SAI3. But SAI1 has four TX RX.
For RT106S ,PDM MIC and audio amplifer use SAI1_RX_DATA0(MIC1) ,SAI1_RX_DATA1(MIC2),SAI2_RX_DATA1(MIC3),SAI3_RX_DATA1(AMP),
For 1060F , PDM MIC and audio amplifer use SAI1_RX_DATA0(MIC1) ,SAI1_RX_DATA1(AMP) ,SAI1_RX_DATA2(MIC2) .
If pdm mic and audio amplifer all ues SAI1RX ,Will there be a problem?
Hi,
1) If pdm mic and audio amplifer all ues SAI1RX ,Will there be a problem?
-- No, it's able to do it.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------