Hi,
We are working with a imx6q custom board with sgtl5000 audio codec. We are using last yocto version, the image is working ok, the audio driver is loaded and we can play wav files using "aplay".
The problem is when we capture audio from Mic or Line. The signal is clipped and the audio captured is horrible. We test a lot of combinations but we couldn't reach any solution.
We see that when we are capturing audio from microphone and increase the capture volume, when the capture level reachs 33 the audio is muted and stops capturing. The same problem happends with the "Mic" input gain, if this value
is greater than 0 the capture is stopped.
The signal is only clipped in the positive part, so we tried to change the ground reference register to see if this was the problem, but it seems not. I attach a picture playing 1Khz tone.
Please, do you have any idea?
Thanks a lot!
Regards,
@
Hi Ivan
sgtl5000 audio codec is not supported in i.MX6 NXP BSPs, but some third party support it:
Microphone input on the SABRE Lite and Nitrogen6x - Boundary Devices
example of dts file : linux-imx6/arch/arm/boot/dts/imx6qdl-sabrelite.dtsi
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you very much for your help ! :smileyhappy:
I took a look again how my dtsi file is, and the only changes are
related with
the mux ports the board is using, but I assume that this configuration
is correct
because the chip can be accessed, I can playback and capture, and change
configuration with alsamixer.
Yesterday we used an old imx53 devel board which mounts a sgtl5000 and
it captures
perfect. I dumped the register configuration and I didn't see any
relevant difference between
both boards.
I reviewed sgtl5000 datasheet and play with the registers related with
gound, reference and
so on, but the input signal was clipped too.
Any idea? Thank you very much
Best Regards
El 08/01/2019 a las 1:58, igorpadykov escribió:
>
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
>
Re: SGTL5000 audio capture problem
reply from igorpadykov
<https://community.nxp.com/people/igorpadykov?et=watches.email.thread>
in /i.MX Processors/ - View the full discussion
<https://community.nxp.com/message/1098193?commentID=1098193&et=watches.email.thread#comment-1098193>
>
Hi Igor,
Thats exactly what I did, dumping the registers in working and not working boards, but I didn't find any relevant difference. Taking a look at the clipped signal it seems it could be a reference or supply problem, but at hardware level
we don't see any problem.
Best regards,