Hi,
I am trying unsuccessfully to bitbake a build for SCM-i.MX6Dual/6Quad (QWKS-SCMIMX6DQ).
I have been following document # SCMIMX6DQLRNUG Rev. 0, 02/2016. See attached tar file
Per the document, in the build machine the following commands have been given:
$ mkdir fsl-arm-yocto-bsp
$ cd fsl-arm-yocto-bsp
$ cp <path to scm package>/meta-fsl-scm.tar.gz .
$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.52-1.1.0_ga
$ repo sync
$ tar zxvf meta-fsl-scm.tar.gz -C sources/
$ DISTRO=fsl-imx-fb MACHINE=imx6dqscm-1gb-qwks source BUILD_DIR=build fsl-setup-release.sh
I have tried both
$ bitbake fsl-image-qt5
and
$ bitbake core-image-base
This is the error that I get:
NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: Command Error: exit status: 1 Output:
Applying patch 0007-MLK-11888-1-arm-imx6-common-fix-ddr_type-identificat.patch
patching file arch/arm/mach-imx/common.h
Hunk #1 FAILED at 181.
1 out of 1 hunk FAILED -- rejects in file arch/arm/mach-imx/common.h
Patch 0007-MLK-11888-1-arm-imx6-common-fix-ddr_type-identificat.patch can be reverse-applied
ERROR: Function failed: patch_do_patch
ERROR: Logfile of failure stored in: /home/grimlock/SnipeBlock3/build/tmp/work/imx6dqscm_1gb_qwks-poky-linux-gnueabi/linux-imx/3.14.52-r0/temp/log.do_patch.32251
ERROR: Task 70 (/home/grimlock/SnipeBlock3/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_3.14.52.bb, do_patch) failed with exit code '1'
Any thoughts what could cause this?
Thanks,
Zeph
Original attachment has been moved to https://community.nxp.com/docs/DOC-337109
解決済! 解決策の投稿を見る。
Hi,
To fix this please try the attached file.
Just replace it on <yocto_installation>sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/ directory
cp –v linux-imx-3.14.52.bbappend <yocto_installation>sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/
This is the main change:
python do_patch_prepend() {
import subprocess
subprocess.call("echo Reseting to rel_imx_3.14.52_1.1.0_ga", shell=True)
subprocess.call("git -C ${S} checkout rel_imx_3.14.52_1.1.0_ga", shell=True)
}
Best Regards,
Alejandro
Hello Zeph,
Please let us know if Alejandro's fix helped.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Work!. Thanks.
Hi,
To fix this please try the attached file.
Just replace it on <yocto_installation>sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/ directory
cp –v linux-imx-3.14.52.bbappend <yocto_installation>sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/
This is the main change:
python do_patch_prepend() {
import subprocess
subprocess.call("echo Reseting to rel_imx_3.14.52_1.1.0_ga", shell=True)
subprocess.call("git -C ${S} checkout rel_imx_3.14.52_1.1.0_ga", shell=True)
}
Best Regards,
Alejandro