SABRESD board 22-pin SATA connector

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRESD board 22-pin SATA connector

461 Views
alanmyler
Contributor II

Hi,

I want to connect an M.2 SATA SSD to the SABRESD board. To do this it appears that I need to use a 22-pin SATA to M.2 adapter. Can I use something like this?

https://www.amazon.co.uk/2-5inch-Adapter-Based-Converter-Card/dp/B08FCZ75M1/

Specifically, will this physically fit ok, as there doesn't appear to be a whole lot of clearance around the 22-pin connector on the board?

Thanks,

Alan

0 Kudos
2 Replies

444 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which i.MX series are you using? The i.mx6q/qp can support SSD device via sata interface

0 Kudos

440 Views
alanmyler
Contributor II

>Which i.MX series are you using? The i.mx6q/qp can support SSD device via sata interface

I'm using the i.MX6QP.

Yes I understood that this processor can support an SSD device via the 22-pin SATA connector.

My question was about how to connect the SSD to the board.

In the meantime I have ordered a 22-bin SATA cable which I believe is the answer to my original question. If not I will follow up with further questions once it arrives and I have a chance to test it.

0 Kudos