SABRE board MCIMX6DL-SDP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE board MCIMX6DL-SDP

653 Views
sudhanshumehta
Contributor IV

I have MCIMX6DL-SDP SABRE board.

I have pre-build image and u boot and i am able to run on the board.

Now I want to make setup on my PC. So that i can write an application.

I have ubuntu 12.0 on my PC.

do we have proper documentation on this?

Thanks

Sudhanshu

Labels (3)
0 Kudos
Reply
1 Reply

401 Views
Yuri
NXP Employee
NXP Employee

Hello,

    Please use information on the Web (about design resources) :

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

The next resources may be useful in application design debugging :

https://community.freescale.com/docs/DOC-103468

https://community.freescale.com/docs/DOC-1490

"AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors."

http://cache.freescale.com/files/32bit/doc/app_note/AN4553.pdf

It may be recommended to apply the recent BSP :

http://www.freescale.com/webapp/Download?colCode=L3.14.38_6UL_LINUX_DOCS&Parent_nodeId=1337699481071...

“Freescale_Yocto_Project_User's_Guide.pdf” describes how to load and build Linux for i.MX6.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply