Hi,
I’m trying to get a Linux image onto SABRE platform MCIMX6DL-SDP. Running Android from the supplied SD card works fine, but I don’t manage to get Linux running. What I did is the following:
[profiles]
chip = MX6DL Linux Update
[platform]
board = SabreSD
[LIST]
name = i.MX6DL-SABRESD-SD
5. Exit MfgTool after „DONE“ is displayed via „Stop“ and „Exit“
6. Swith SW6 to “01000010”
7. Restart the board
Output:
U-Boot 2009.08 (Aug 16 2013 - 12:25:07)
CPU: Freescale i.MX6 family TO1.1 at 792 MHz
Thermal sensor with ratio = 186
Temperature: 43 C, calibration data 0x5975245f
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 198000000Hz
emi_slow clock: 99000000Hz
ddr clock : 396000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6DL/Solo-SABRESD: unknown-board Board: 0x61011 [POR ]
Boot Device: SD
I2C: ready
DRAM: 1 GB
MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3
*** Warning - bad CRC or MMC, using default environment
In: serial
Out: serial
Err: serial
Found PFUZE100! deviceid=10,revid=11
Net: got MAC address from IIM: 00:04:9f:02:e4:28
FEC0 [PRIME]
Hit any key to stop autoboot: 0
FEC: Link is down 7949
Using FEC0 device
TFTP from server 192.168.1.101; our IP address is 192.168.1.103
Filename 'uImage'.
Load address: 0x10800000
Loading: FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
…
It seems as if U-Boot is looking for the OS via Network, can I change this somehow?
Also, I can’t stop autobooting by hitting any key (power, volume up/down)…
I used the manuals “i.MX_6DualQuad_SABRE-SD_Linux_Users_Guide.pdf” or “i.MX Development Quick Start-FAE-V3.pdf” – did I use the wrong manuals or do something else wrong?
Kind regards,
Markus
解決済! 解決策の投稿を見る。
I've finally found out the solution myself:
The U-Boot environment variable was incorrectly set. Setting it to
bootargs=console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale
loadaddr=0x10800000
bootargs_base=setenv bootargs console=ttymxc0,115200
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24
bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 2;mmc read ${loadaddr} 0x800 0x2000;bootm
bootcmd=run bootcmd_mmc
made Linux boot with no problems.
Maybe someone could update the MfgTool or the manuals accordingly?
Kind regards,
Markus
I've finally found out the solution myself:
The U-Boot environment variable was incorrectly set. Setting it to
bootargs=console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale
loadaddr=0x10800000
bootargs_base=setenv bootargs console=ttymxc0,115200
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24
bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 2;mmc read ${loadaddr} 0x800 0x2000;bootm
bootcmd=run bootcmd_mmc
made Linux boot with no problems.
Maybe someone could update the MfgTool or the manuals accordingly?
Kind regards,
Markus
Another thing comes to my mind: I use a 16GB SDHC card. Does this make any parameter changes necessary?
Kind regards,
Markus