S/W encoding H.264 with i.MX7D

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S/W encoding H.264 with i.MX7D

ソリューションへジャンプ
1,020件の閲覧回数
ScottKerstein
Contributor III

Hello,

Looking to encode H.264 from a 1080p30fps imager on the i.MX7D using GStreamer.  Is there a way to determine the CPU utilization and if a Cortex-A7 running at 1.2GHz is enough to do this task?  This is the only task.  

Thanks, in advance.

Scott

ラベル(4)
0 件の賞賛
1 解決策
872件の閲覧回数
ScottKerstein
Contributor III

Thanks, Igor.  Looks like it will be limited to just JPEG in software.

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
872件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Scott

nxp linux video performance without vpu is described in attached Release Notes

Table 31. Video codec specification for hardware without VPU acceleration.

More details about VPU versus non-VPU analysis  can be obtained creating service request

Support|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
873件の閲覧回数
ScottKerstein
Contributor III

Thanks, Igor.  Looks like it will be limited to just JPEG in software.

0 件の賞賛