Hello All,
I need to rotate YUV422 data..I have applied rotation using Following code. My input image size is 1024*768 and it is non interleaved YUV 422 data.
I am applying rotation on this buffer. I am not getting correct output...IPU gives output with corruption. I am attaching both input and output YUV422 images for reference.
Please help me to get the correct if there are any mistake i made in DMA channel setup.
Following i s the code snap i am using for rotation...I am using Platform SDK as reference code and all my code for IPU driver is based on Platform SDK V1.1.0
Thanks
John.
=================================================================================================================
// PP task.
rot_chnl_in = MEM_TO_IC_PP_ROT_CH47;
rot_chnl_out = IC_PP_ROT_TO_MEM_CH50
memset(&rot_info, 0x00, sizeof(ipu_rot_info_t));
rot_info.width_in = panel->width;
rot_info.height_in = panel->height;
rot_info.width_out = rot_info.height_in;
rot_info.height_out = rot_info.width_in;
rot_info.strideline_in = rot_info.width_in * 2;
rot_info.strideline_out = rot_info.width_out * 2;
rot_info.pixel_format_in = NON_INTERLEAVED_YUV422;
rot_info.pixel_format_out = NON_INTERLEAVED_YUV422;
rot_info.rot = 1;
rot_info.hf = 0;
rot_info.vf = 0;
rot_info.addr0_in =rot_in_mem;
rot_info.addr0_out = rot_out_mem;
ipu_rotate_idmac_config(ipu_index, rot_chnl_in, rot_chnl_out, rot_info);
ipu_ic_rotation_config(ipu_index, taskType, 1, 0, 0);
//enable ic task
ipu_ic_task_enable(ipu_index, taskType, IC_PP, 1);
ipu_ic_task_enable(ipu_index, taskType, IC_ROT, 1);
ipu_ic_enable(ipu_index, 1, 1);
//enable rotate idma channel
ipu_channel_buf_ready(ipu_index, rot_chnl_out, 0);
ipu_channel_buf_ready(ipu_index, rot_chnl_in, 0);
while (ipu_idmac_channel_busy(1, rot_chnl_in)) ;
while (ipu_idmac_channel_busy(1, rot_chnl_out))
Original Attachment has been moved to: input.yuv.zip
Original Attachment has been moved to: output.yuv.zip
The trick is to set the U offset. Since the image is planar (non_interleaved) we can see it as three separate buffers: Y buffer, U buffer and V buffer. However, we need to indicate how far (the offset) the U buffer and Y buffer are from the Y buffer. Actually set the u offset is enough.
Check the next config I used to perform first re-sizing and then rotation
memset(&res_info, 0x00, sizeof(ipu_res_info_t));
res_info.width_in = panel->width;
res_info.height_in = panel->height;
res_info.height_out = panel->width;
res_info.width_out = panel->height;
res_info.strideline_in = res_info.width_in;
res_info.strideline_out = res_info.width_out;
res_info.pixel_format_in = NON_INTERLEAVED_YUV422; // INTERLEAVED_RGB565;
res_info.pixel_format_out = NON_INTERLEAVED_YUV422; // INTERLEAVED_RGB565;
res_info.addr0_in = res_in_mem;
res_info.addr0_out = res_out_mem;
res_info.u_offset_in = 0xc0000; // hardcoded for a 1024 x 768 image
res_info.u_offset_out = 0xc0000;
ipu_resize_idmac_config(ipu_index, res_chnl_in, res_chnl_out, res_info);
//set rotate idma
memset(&rot_info, 0x00, sizeof(ipu_rot_info_t));
rot_info.width_in = panel->height;
rot_info.height_in = panel->width;
rot_info.width_out = panel->width;
rot_info.height_out = panel->height;
rot_info.strideline_in = rot_info.width_in;
rot_info.strideline_out = rot_info.width_out;
rot_info.pixel_format_in = NON_INTERLEAVED_YUV422; //INTERLEAVED_RGB565;
rot_info.pixel_format_out = NON_INTERLEAVED_YUV422; //INTERLEAVED_RGB565;
rot_info.rot = 1;
rot_info.hf = 0;
rot_info.vf = 0;
rot_info.addr0_in = res_out_mem;
rot_info.addr0_out = rot_out_mem;
rot_info.ubo_in = 0xc0000;
rot_info.ubo_out = 0xc0000;
ipu_rotate_idmac_config(ipu_index, rot_chnl_in, rot_chnl_out, rot_info);
If you want to try on Linux, you can execute the overlay unit test:
root@freescale /unit_tests$ ./mxc_v4l2_overlay.out -r 4
The -r parameter makes the camera rotate according to the rotate mode number. I have just tried and it works.
Rgds
Rogerio
Hi John,
The unit tests comes with the BSP (LTIB or YOCTO). The binaries are located at rootfs/unit_tests and the source code you can get with the LTIB command:
./ltib -p imx-test -m prep
the source will be located at <ltib folder>/rpm/BUILD/imx-test-<version>
I don't know how to extract the source using YOCTO, but it should be something like this: bitbake imx-test
Rgds
Rogerio
HI Rogerio
Thanks for your reply. Are you referring to which ready driver? Are you referring to V4l2 driver? Actually we are building system around Platform SDK and that's why we are using IPU source code from SDK.
Can you guide me on the line of platform SDK IPU source code? can we rotate YUV422 data using above mentioned code?
Thanks again....
John.
hi rogerio,
appreciate if you could advice on how to rotate a video recorded by ov5640_mipi camera sensor on the Linux driver or camera hal layer?
my h/w platform is imx6q-based custom board with freescale r13.4.1 BSP.
Thanks!
Hi john_ortega,
What rotation do you need? 90? 180? Flip? all of them?
I'm asking because if you only need flip, it´s possible to do simply changing the IDMAC config and I guess even the current framebuffer driver supports it, if you need other rotations, you will need to involve Image Converter block to do it.
Rgds
Rogerio