Rise/fall time spec of MIPI CSI HS Line Receiver in i.MX7D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Rise/fall time spec of MIPI CSI HS Line Receiver in i.MX7D

Jump to solution
1,015 Views
ko-hey
Senior Contributor II

Hi all

Could someone tell me whether the HS line receiver has rise/fall timing spec or not ?

I'm checking a mipi-csi timing spec with custom board which has i.MX7D.

According to the table 77 of IMX7DCEC Rev. 4, there are no timing spec for rise and fall time in HS Line Receiver.

However, I heard the mipi compliant test has the spec for rise and fall time.

Are there no rise and fall timing spec for HS Line Receiver ?

Ko-hey

Labels (3)
0 Kudos
1 Solution
840 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

you are right, there is no rise and fall timing spec for HS Line Receiver,

mipi specification defines it only for transmitter.

Best regards
igor
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
841 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

you are right, there is no rise and fall timing spec for HS Line Receiver,

mipi specification defines it only for transmitter.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos