Resize weston/wayland screen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Resize weston/wayland screen

7,995件の閲覧回数
stasgil
Contributor III

Hi everyone,

Please bear with me because i have no experience or knowledge of how all the graphical backends (wayland x11 etc) work or how weston relates to them, or how displaying stuff really works, so thank you for your patience.

We are using imx6 dual-lite chip for our custom board, and 320x240  ILI9341V  display. Prototyping was done on the Sabre-sd dev board, so bsp was pretty much copied from there. We've had some troubles getting the display to run, but it is running now, however, (i'm not sure how to exactly describe it) the "virtual screen size" seems to be a lot bigger than the actual display size, so for example if I open a shell window, only part of it will be visible on the display. 

I know the screen itself is run in rc script by "openvt -s weston -- $OPTARGS"

$OPTARGS don't contain anything, but i'm pretty sure the backend that is being used at the moment is fbdev.

Does anyone have any pointers on what should i do or look at to get the screen to match the display size ? I am not sure which information i should provide, so let me know if there's something i can give. Here are some hopefully relevant outputs:

root@imx6dlsabresd:/# fbset

mode "240x320-69"
# D: 6.750 MHz, H: 23.438 kHz, V: 69.137 Hz
geometry 240 320 240 320 16
timings 148148 24 8 6 3 16 10
vsync high
rgba 5/11,6/5,5/0,0/0
endmode

root@imx6dlsabresd:/# weston-info
interface: 'wl_compositor', version: 3, name: 1
interface: 'wl_subcompositor', version: 1, name: 2
interface: 'wl_scaler', version: 2, name: 3
interface: 'presentation', version: 1, name: 4
presentation clock id: 4 (CLOCK_MONOTONIC_RAW)
interface: 'wl_data_device_manager', version: 2, name: 5
interface: 'wl_shm', version: 1, name: 6
formats: RGB565 XRGB8888 ARGB8888
interface: 'wl_viv', version: 1, name: 7
interface: 'wl_viv', version: 1, name: 8
interface: 'wl_output', version: 2, name: 9
x: 0, y: 0,
physical_width: -1 mm, physical_height: -1 mm,
make: 'unknown', model: 'DISP3 BG',
subpixel_orientation: unknown, output_transform: normal,
mode:
width: 240 px, height: 320 px, refresh: 75 Hz,
flags: current preferred
interface: 'wl_seat', version: 4, name: 10
name: default
capabilities: touch
interface: 'wl_input_panel', version: 1, name: 11
interface: 'wl_input_method', version: 1, name: 12
interface: 'wl_text_input_manager', version: 1, name: 13
interface: 'wl_shell', version: 1, name: 14
interface: 'xdg_shell', version: 1, name: 15
interface: 'desktop_shell', version: 3, name: 16
interface: 'workspace_manager', version: 1, name: 17
interface: 'screenshooter', version: 1, name: 18

When i run weston-fullscreen, the window that shows up on the display says

Surface size: 640, 480

Scale: 1, transform: 0

Fullscreen: 0

(but then it seems to request a keyboard input, which we don't have so it seems that i can't actually use the tool.)

fb related tests in /unit_tests seem to pass fine.

Thanks for your time !

ラベル(4)
タグ(3)
0 件の賞賛
3 返答(返信)

2,143件の閲覧回数
r_trivedi123
Contributor IV

@stasgil, Hope our created plugin can help for your needs,

sisigaylandsink - A custom gstreamer plugin to control geometry 
Features and demo is provided in the video link.

--
BR
rutvij.trivedi@siliconsignals.io

0 件の賞賛

4,973件の閲覧回数
b36401
NXP Employee
NXP Employee

Here are documentation regarding to Wayland/Weston on i.MX6:

https://community.nxp.com/docs/DOC-332151
https://community.nxp.com/docs/DOC-95380

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

4,972件の閲覧回数
stasgil
Contributor III

Thanks, I cannot access the first link you have provided however "This place or content does not exist or access to it is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here."

0 件の賞賛