Resize SD card partition on imx8qxp of Yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Resize SD card partition on imx8qxp of Yocto

2,558件の閲覧回数
liuyonggang
Contributor III

Platform:imx8qxp

Environment:Yocto

   currently,I build SD image in Yocto environment.I use dd comand burn SD image into SD card.It was successful and I will found two partitions on SD card.But I have a question.I want to change previous two partition sizes and add a partition at build time.Where can I modify it.

      Tks

BRs

Johnny

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,446件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the chapter 4.3.3 Partitioning the SD/MMC card of enclosed file

0 件の賞賛
返信

2,446件の閲覧回数
liuyonggang
Contributor III

Hi Xie,

      I want to change previous two partition sizes and add a partition at build time,other than using fdisk command manually.

      Tks

BRs

Johnny

0 件の賞賛
返信

2,446件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you can find your sdcard layout here, then you can set as you need,generate new class file

meta-fsl-arm/image_types_fsl.bbclass at master · Freescale/meta-fsl-arm · GitHub 

2,446件の閲覧回数
liuyonggang
Contributor III

Hi Joan,

      Tks for your comments.

      I have solved this issue last week.

      Your advice is correct.

BRs

Johnny

0 件の賞賛
返信