Reset pin on JTAG unavailable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reset pin on JTAG unavailable

495件の閲覧回数
vivekvix
Contributor II

vivekvix_0-1702548918187.png

The above image shows the JTAG pins from the IMX8MP Processor

vivekvix_3-1702548984954.png

The above shows the image of the JTAG connector which we are using, which contains the RESET pin. 

We have used the NXP provided pin config tool, but the reset pin for the same is not available.
The image for which is also attached below. 
Pls note that there is no JTAG_RESET on the IMX8mp whereas there is a JTAG_RST on the connector.

vivekvix_2-1702548929738.png

 

What is the reset mechanism used for resetting while using JTAG?
Please provide us the solution for the same

 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

472件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

462件の閲覧回数
vivekvix
Contributor II

I have gone through the link
But it shows how nRST can be used for boundary scan. 

I want to know how the reset functionality can be implemented...

0 件の賞賛
返信