Required very low power processor for battery operated device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Required very low power processor for battery operated device

1,233 次查看
mrudangshelat1
Senior Contributor II

Hi,

I am looking for a very low power processor solution for battery-operated medical devices. Earlier I have used i.MX6ULL but the DRAM and eMMC combined MCP package is EOL now and needs to change the processor part to support LPDDR3 or LPDDR4 compatible. It also should have 3xSAI, 4xUART, SPI, and I2C interfaces. I am looking for an i.MX7/8 based solution.

Regards,

Mrudang

0 项奖励
回复
6 回复数

1,109 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

one can look at i.MX comparison tables seems i.MX7D best choice:

https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf 

https://www.nxp.com/docs/en/supporting-information/IMX8LAYERCMPR.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,109 次查看
mrudangshelat1
Senior Contributor II

Hi Igor,

We have a 3 x 120mAh battery in current i.MX6ULL+M4 based MT2523 (MediaTek FPU) based device. And it provides battery back-up 9-10 days. Please see below the table of power consumption for your reference. Will i.MX7D can provide such battery back-up? 

Sr#Peripheral DescriptionPart#ManufacturerQtyVoltage Rails (Volt)Component Power (mW)
1.01.83.33.75.0
1Microprocessor
(Cortex A7)
MCIMX6Y1CVK05AANXP159.4000 8.6061  100.9700
2Sensor Hub
(Cortex M4)
MT2523DMediaTek1   2.0659 8.7906
3eMMCMT29PZZZ4D4BKESK-18 W.94HMicron1 22.500050.0000  236.3250
4LPDDR2 RAM1 16.6667   34.5000
5EEPROM24AA32AMicrochip1 0.4000   0.8280
6M2M ModuleLE866Telit1   550.0000 2340.2500
7BLE ModuleUGMZ2AAALPS1  6.0000  22.7700
86DOF- Acc + GyroLSM6DSMST Microelectronics1 0.6500   1.3455
93DOF-MagnetoLIS3MDLST Microelectronics1 0.00100.2700  1.0267
10Skin Side Mic-AMP34DB02TRST Microelectronics1 0.6500   1.3455
11Mic-A PDM to I2S Con ADAU7002Analog Device1 0.6700   1.3869
12Skin Side Mic-BMP34DB02TRST Microelectronics1 0.6500   1.3455
13Mic-B PDM to I2S ConADAU7002Analog Device1 0.6700   1.3869
14Outside MicWM7216ECirrus Logic1 0.9800   2.0286
15Outside Mic PDM to I2S ConADAU7002Analog Device1 0.0015   0.0031
16Temperature SensorSi7051Silicon Labs1  1.1100  4.2125
17Vibration ActuatorZ4FC1B1301781KOTL1  110.0000  417.4500
18Actuator DriverDRV8601Texas Instrument1  1.7000  6.4515
19RTCAM0805Ambiq Micro1 0.0033   0.0068
20Battery ChargerBQ24074Texas Instrument1   5.00002.000032.7750
21Fuel GaugeMAX17050Maxim Integrated1   0.0250 0.1064
22PMICMC32PF3000A6EPNXP1   2.0000 8.5100
23Push ButtonSW1, SW2, SW3 3 1.0000   6.2100
24LEDsLED1, LED2, LED3 3  2.0000  22.7700
  Max Rail Current Requirement 59.400044.8425179.6861559.09092.0000 
 Total System Power Consumption(mW)     3252.7945

Regards,

Mrudang

0 项奖励
回复

1,109 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

some typical power consumption figures can be found in

i.MX 7DS Power Consumption Measurement

However for your specific case you should produce prototype board

and measure power consumption for specific application requirements.

Best regards
igor

0 项奖励
回复

1,109 次查看
mrudangshelat1
Senior Contributor II

Hi Igor,

So, I can use iMX7S, right?

Mrudang

0 项奖励
回复

1,109 次查看
igorpadykov
NXP Employee
NXP Employee

yes Mrudang

Best regards
igor

 

0 项奖励
回复

1,109 次查看
mrudangshelat1
Senior Contributor II

Hi Igor,

Let me check and let you know ASAP.

Mrudang

0 项奖励
回复