Request for i.MX535 Performance Benchmark Document

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Request for i.MX535 Performance Benchmark Document

650件の閲覧回数
SrideviK
Contributor III

Hi,

Pls share the i.MX535 Performance Document or Report (either Sabre / EVK) for our benchmarking.

Need to understand the peripheral access speed achieved for Micro-SD/eMMC/USB, etc.

Regards,

Sridevi

0 件の賞賛
返信
2 返答(返信)

545件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Sridevi,

You can go to http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&nodeId=018rH3ZrDR988D&fpsp=1&... to download the IMX53RM. The details of performance and peripheral speed access you can see in it. Hope this can help you ~~

Best Regards

Dan


0 件の賞賛
返信

545件の閲覧回数
SrideviK
Contributor III

Thanks Dan for the reply.

My device is based on i.MX535 (Android2.3.7 platform). The design is done almost similar to the i.MX535 based Sabre / QSB.

I need to evaluate the performance of all the interfaces in my device.

For this I would need the practical performance report for the processor interfaces - so i.MX535 based Sabre / QSB performance report would be suitable for the same.

Hope the interface performances would have been evaluated using some tools.

Pls share the relevant document for benchmarking.

Regards,

Sridevi

0 件の賞賛
返信