Register setting and voltage supply of NVCC_USB_H

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Register setting and voltage supply of NVCC_USB_H

609件の閲覧回数
ko-hey
Senior Contributor II

Hi all

Please teach me the register setting and voltage supply of NVCC_USB_H.

I understand that NVCC_USB_H can be connected to I2C power rail from following thread.

I guess it's same as case of using GPIO.

Question, i.MX6SoloX power design 

I want to use "USB_H_DATA" and "USB_H_STROBE" pin as 1.8 V level GPIO.

According to the table 10 of IMX6SXCEC, the NVCC_USB_H pin specification is as below.

pastedImage_2.png

Do I need to set the register when I use "USB_H_DATA" and "USB_H_STROBE" pin as 1.8 V level GPIO ?

Ko-hey

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

486件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

this table is correct, you can set register as table shows.

0 件の賞賛
返信

486件の閲覧回数
ko-hey
Senior Contributor II

I know the table is correct.

My question is do I need to set the DDR_SEL field of IOMUXC_SW_PAD_CTL_PAD_USB_H_DATA register to "11” when I use the pin as a 1.8V GPIO ?

I can't understand that why the pins related to the DDR.

Ko-hey

0 件の賞賛
返信

486件の閲覧回数
ko-hey
Senior Contributor II

joanxie

Could you follow the above question ?

Ko-hey

0 件の賞賛
返信