Hi community,
I have some questions about i.MX6DQ Linux BSP (L3.0.101) frame buffer.
[Q1]
You know /dev/fb0 is unblanked when i.MX6DQ Linux BSP (L3.0.101_4.1.1) is boot, but /dev/fb2 is blanked if fb0=ldb and fb2=hdmi.
(with 'video=mxcfb0:dev=ldb video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB' boot parameter)
Then, we want to be unblanked both display (lvds and hdmi) when boot i.MX6DQ Linux BSP, not only /dev/fb0.
I checked Dual display LVDS + HDMI on iMX6 , but it seems to has been unresolved.
So what should we modify to realize it?
Change a device driver? or a boot parameter?
[Q2]
We can unblank a hdmi display with the following command.
echo 0 > /sys/class/graphics/fb2/blank
After unblanking both display (/dev/fb0:lvds, /dev/fb2:hdmi) by the above command, I executed the following command.
echo 1 > /sys/class/graphics/fb0/blank
Then, not only fb2 (hdmi display) was blanked but also fb0 (lvds display).
How should we do to blank only fb2 in this case?
Best Regards,
Satoshi Shimoda
解決済! 解決策の投稿を見る。
For Q1, you can add "echo 0 > /sys/class/graphics/fb2/blank" at the end of rootfs//etc/rc.d/rc.local
For Q2, it is more like backlight issue. You can modify "drivers\video\backlight\pwm_bl.c", function pwm_backlight_check_fb(), just return 0 from it.
For Q1, you can add "echo 0 > /sys/class/graphics/fb2/blank" at the end of rootfs//etc/rc.d/rc.local
For Q2, it is more like backlight issue. You can modify "drivers\video\backlight\pwm_bl.c", function pwm_backlight_check_fb(), just return 0 from it.