Hi aLL,
I was able to run QT demo's created by LTIB. Though the project i created doesnt run on my IMX 6. When i select qmake file from /qt-everywhere-opensource-src/bin/qmake i am getting an ERROR.
"QT version not properly Installed, please run Make Install"
am i selecting the wrong qmake file??
Kindly advice
Hi Vishvapathi,
you can also use LTIB to compile your project.
<ltib-home>/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/demos
Make some changes to demos.pro file ,as add our project name in SUBDIRS
Ex: SUBDIRS = \ demos_shared \
demos_deform \
demos_gradients \
…………………
demos_<your Qt project>
Ex: <ltib-home> /rpm/Build/qt-opensource4.6.0/demos.
Thanks & Regards,
Raybiztech.
Hi,
My QT application and touch screen are working now. but for building ltib its taking a lot of time even for a small change in QT project. Is there any alternate way for deploying qt ?
Kindly advice
Hi,
./ltib -m prep -p qt-embedded.spec
Processing: qt-embedded
=========================
Build path taken because: directory build, build key set,
Cowardly refusing to clobber existing directory:
/home/vishva/Desktop/L3.0.35_4.0.0_130424_source/yes/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0
Remove this by hand if you really want to rebuild this package from scratch
f_prep() returned an error, exiting
traceback:
main:572
Exiting on error or interrupt
is there a way to make it work without deleting the files in BUILD/????
Hi Vishvapathi,
No need of doing prep again. After following the process which i mentioned in previous reply, just cd to your LTIB path and do ./ltib it will build your project. Keep a watch on your debug log whether your project is building or not.
Thanks & Regards,
Raybiztech.
Hi,
I followed the ur instruction and i am able to deploy qt application in my IMX, mistake was mine. I copied the wrong folder.
My application is working, but mouse click events are not working for qt application. Do i have to configure anything for using mouse+qt?
Kindly advice
wen i tried cat /dev/input/mouse1 i was getting some funny characters so i guess the mouse is working fine.