Hi Community,
For an imx6qsabresd board : I would like to implement the Redundant Boot Support.
I modified the secondary image table format like this in my sdcard to reboot with the first u-boot after a WARM reset.
Address | Value |
---|---|
0x200 (reserved Chip Num) | 0 |
0x204 (reserved Drive Type) | 0 |
0x208 (tag) | 0x00112233 |
0x20C (first sector number) | 0x002 |
0x210 (reserved Sector Count ) | 0 |
I wrote this header in 0x200 :
0000 0000 0000 0000 3322 1100 0200 0000
0000 0000
dd if=header of=/dev/sdb bs=1 seek=512 count=20
For rebooting with this table I created a WARM reset in u-boot :
PERSIST_SECONDARY_BOOT : SRC_GPR10[30]
reg = readl( &psrc->gpr10 );
reg |= 0x40000000;
writel( reg , &psrc->gpr10 );
I send a reset in u-boot prompt and the system do nothing :
=> reset
resetting ...
1) The secondary image table is correct ?
2) The WARM reset cannot be like that ?
As imx6 redundant boot from secondary bootloader may be useful for someone , i am sharing below procedure which worked for me .
Create primary boot image
dd if=u-boot.bin of=/dev/sdc bs=1K seek=1 skip=1
Create secondary boot image, in this example, start from 400KB i.e seek in blocks.
dd if=u-boot-sec.bin of=/dev/sdc bs=512 seek=800
Take header file shared in below link.
i.MX53 Redundant Boot -blog archive
To create secondary image table, run below command
dd if=header of=/dev/sdc bs=512 seek=1count=1
Destory primary u-boot by setting the entry of ivt to 0, so rom can jump to secondary image.
dd if=/dev/zero of=/dev/sdc bs=1 seek=1028 count=4
for imx6 check value at 0x20d8044 it should show 0x40000000 , which indicates imx6 has booted from secondary bootloader.
I can suspect that there is some mishmash with big- and litte-endian modes.
Please doublecheck this "header" file with "hexdump -C" command.
Here is an example of mishmash I mean:
# echo -n @ABC > a
# hexdump -C a
00000000 40 41 42 43 |@ABC|
00000004
# hexdump a
0000000 4140 4342
0000004
#
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I can confirm that it's not working on imx6qsabresd with sd-card.
Tried every possibility regarding endianness, different sector offsets, etc.
Since this feature is a must-have in our product, I shall appreciate it that a freescale engineer can take this topic up.
Are we facing a silicon bug? Is the programming manual lacking information? Or do we miss something else?
Best regards,
Wim