Hi ,
Firstly, thank you for coming here, please help solve the following problems.
Yocto version : fsl-yocto-L4.1.15_2.0.0-ga
Linux Kernel Version:4.1.15
My Question:
The rootfs I generated with yocto was very large, and I carefully checked that there were a lot of debugging software and other unrelated libraries that I didn't need. I want to trim the file system, but I don't know what instructions or recipes I should run, please help me solve this problem.
Thank you !
已解决! 转到解答。
Hello Zhang Ying,
You would need to replace <image> with the recipe for your image, not the resulting file system. In this example fsl-image-qt5.
You could just run:
$ bitbake -g fsl-image-qt5 && cat pn-buildlist
But for ease the command filters the packages maked as “native” and sorts them so they are in alphabetical order and only the unique results.
I hope this helps!
Regards,
Hi,
1. As you said, I entered the command line and it appears as follows:
Thank you
Best regards
Hello Zhang Ying,
The bitbake command should be run on the host while the bitbake environment is setup.
Hplip available on the BSP but you would need to refer to CUPS and HPlib documentation for details of how it works. You may also post a new thread regarding this so more Community users can see it and maybe collaborate with an answer.
Regards,
Hello Zhang Ying,
Which rootfs did you bake?
You could start from the bigger image and remove packages, or you could start from the core-image-minimal and add packages as needed.
If you need a graphical interface I would suggest the first approach, starting with the larger image with all required libraries and dependencies and removing the unwanted packages.
You can list all packages of an image with the command:
bitbake -g <image> && cat pn-buildlist | grep -ve "native" | sort | uniq
And then work from there removing unnecessary packages by adding the following line on the conf/local.conf file inside the build directory like so:
IMAGE_INSTALL_remove += “ package package1 package2”
I hope this helps!
Regards,
Hello Zhang Ying,
You would need to replace <image> with the recipe for your image, not the resulting file system. In this example fsl-image-qt5.
You could just run:
$ bitbake -g fsl-image-qt5 && cat pn-buildlist
But for ease the command filters the packages maked as “native” and sorts them so they are in alphabetical order and only the unique results.
I hope this helps!
Regards,