Read IMX6ULZ fusemap

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Read IMX6ULZ fusemap

740 次查看
jupiter_hce
Contributor III

Hi,

I've read the i.MX 6ULL Reference Manual, the UNIQUE_ID can be read at fuse address 0x410[10:0] and 0x420[15:11], how to inteprete following fusemap to find  the address and value of x410 and 0x420?

0000000 0003 0032 7059 625d 59d2 432b 0038 7130
0000010 0002 0043 0000 0000 0000 0000 0000 0000
0000020 0000 0000 0000 0000 004c 0000 0000 0000
0000030 0000 0000 0000 0000 cf5f 5474 0000 0000
0000040 bada bada bada bada bada bada bada bada
*
0000060 0000 0000 0000 0000 0000 0000 0000 0000
*
0000080 0000 0000 0000 0000 0fbf 9f05 0004 0fc0
0000090 9f05 0004 bada bada 4100 0000 0000 0000
00000a0 0000 0000 0000 0000 0000 0000 0000 0000
00000b0 0000 0000 0040 0000 0002 0000 0000 0000
00000c0 0000 0000 0000 0000 0000 0000 0000 0000
*
0000100

Thank you.

Kind regards,

- jupiter

标签 (3)
0 项奖励
回复
1 回复

637 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jupiter

one can look at:

Burning eFuses on i.MX6 and i.MX7 - i.MXDev Blog 

https://community.nxp.com/docs/DOC-95458 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复