Re: mfgtool imx8mq evk fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: mfgtool imx8mq evk fails

407 Views
dariusz_kazmier
Contributor I

Hi,

I have the same problem.

I want to reinstall my imx8 board bud I have got error:

error.jpg

First installation was done and works correctly, but I have to reinstall system, and now I can't do it?

I use the same port, PC etc.

Where is a problem?

0 Kudos
1 Reply

365 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   The i.MX8 board should be in Serial (USB) Downloader Boot Mode.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos