Re: Altium for the i.MX 8M EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Re: Altium for the i.MX 8M EVK

3,795 次查看
richardg
Contributor II

Hi Yuri,

I would very much appreciate it if you could send me the altium design files for the imx8M mini Eval kit as well. Schematic and layout if you could.

Best regards,

Richard.

14 回复数

2,118 次查看
deepak2298
Contributor I

Hello Yuri,

 

Can you send me design files in .alg or Altium design files format on my email "deepak.kr@noccarc.com"

0 项奖励

3,416 次查看
bastien
Contributor I

Hello,

This topic could be useful to the readers if the files are downloadable.

Can we have the .ALG file to import in Altium DESIGNER ?

Many thanks

Best regards

0 项奖励

3,374 次查看
Yuri
NXP Employee
NXP Employee

@bastien 

Hello,

  I've sent You file directly.

Regards,
Yuri.

0 项奖励

943 次查看
Zater
Contributor II

Hello Mr. Yuri 

Can you please  send me the alg file to my email :
amer.zater@OptimusDoruk.com

0 项奖励

3,168 次查看
emagnioj
Contributor II

Hello, i m looking for Altium Designer version of 8MNANOD4-EVK reference project. ( LPDDR4 )

is it available?

Thank you in advance,

Dom

0 项奖励

3,148 次查看
Yuri
NXP Employee
NXP Employee

@emagnioj 
Hello,

  I can send You the 8MNANOD4-EVK files, which customers can try to import by Altium.
Please create separate thread /  request for it.

 

https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu

 

Regards,
Yuri.

0 项奖励

3,425 次查看
richardg
Contributor II

Hi NXP

 

Does anyone from NXP monitor these posts?

4 weeks ago I asked if you have Altium design files for the Imx8M Mini eval kit. No one from NXP has replied. 

I have managed to convert the schematics you have provided, but the PCB files will not succesfully convert on even the latest versions of Altium !

Are the files that NXP provide in the 8MMINILPD4-EVK-DESIGNFILES.zip  Folder Allegro PCB files? Altium does not recognise them as such.

I would very much appreciate it if someone at NXP could send me Altium design files for the imx8M mini Eval kit, or provide alternative PCB  design files that Altium can convert  - OrCAD would be fine.

It appears that I am not the ony one with this issue.

 

Best regards,

 

Richard.

0 项奖励

3,425 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   Looks like this request was lost. 

If possible, please create non Community case \ ticket.

https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu  

Regards,

Yuri.

0 项奖励

3,424 次查看
richardg
Contributor II

Uri has finnaly provided me with Allegro PCB files that will convert within Altium. Thank you.

These need to be the .ALG files, not the .BRD files.

Uri, could you put the .ALG files in the on-line design files ZIP package so all the others that have this issue can convert the files?

Regards,

Richard.

0 项奖励

3,424 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   Design files are provided by NXP in formats, which are used by design engineers,

assuming, that conversion  to other formats should be performed by customers, if needed. 

Regards,

Yuri.

0 项奖励

3,424 次查看
richardg
Contributor II

Hi Yuri,

Many design engineers use Altium.

The Allegro layout files you supply on your website in 8MMINILPD4-EVK-DESIGNFILES.zip cannot be converted within Altium. I am not the only one who has had this problem.

I am strongly suggesting that you include the .ALG files that you recently sent me, in the online ZIP file so that other Altium users can obtain the pcb DATA.

This would be of conciderable help to Altium users who want to design a imx8M-mini based system.

Best regards,

Richard.

3,424 次查看
carlesre
Contributor II

Dear Richard,

would you be so kind to share Altium files with me?

I would really appreciate that.

carles.recasens@wallbox.com

Thank you in advance!

0 项奖励

3,424 次查看
Yuri
NXP Employee
NXP Employee

I've sent some comments directly.

0 项奖励

1,265 次查看
johnkilovych
Contributor I

Hi!

 

Please share .alg file for me as well

 

johnkilovych@gmail.com

 

0 项奖励