I am considering to use i.MX6DL (Yocto Linux kernel 3.10) with AR0330 camera sensor connected via MIPI interface.
The camera operation mode is following:
lanes = 2-lanes mipi
pixel format = Raw RGB (Bayer RGGB) 10-bit
Fserial = 480Mhz
PixelRate = 98 Mpixel/s
Does anyone know if i.MX6DL is able to handle this configuration?
HI Anton
I think it may be supported, MIPI CSI-2 main characteristics are given on p.68
presentation below
A Deep Dive into Image Processing for i.MX 6 Series Applications Processors
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for your prompt answer.
Special thanks for the presentation which was extremely helpful!
In fact, based on the reference manual and on the presentation, there is a possibility to implement the operation mode mentioned in my question.
Thanks again and best regards,
Anton