RTL8201 for i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTL8201 for i.MX6

1,697件の閲覧回数
wilsonlin
Contributor I

Hi all

I use Realtek RTL8201FN on i.MX6.

I'm following this to setup the chip clock to 50MHz.

(Use pin MX6Q_PAD_RGMII_TX_CTL__ENET_ANATOP_ETHERNET_REF_OUT)

https://community.freescale.com/message/346089#346089

I check mii info

MX6Q U-Boot > mii dev

MII devices: 'FEC0'

Current device: 'FEC0'

MX6Q U-Boot > mii info

PHY 0x00: OUI = 0x0732, Model = 0x01, Rev = 0x06, 100baseT, FDX

PHY 0x01: OUI = 0x0732, Model = 0x01, Rev = 0x06, 100baseT, FDX

Why do I have  two device PHY0 and PHY1?

I ping my server 192.168.1.2 but it's not work.

MX6Q Mlot U-Boot > ping 192.168.1.2

FEC: Link is Up 786d

Using FEC0 device

ping failed; host 192.168.1.2 is not alive

My IOMUX setting:

iomux_v3_cfg_t enet_pads[] = {

  MX6Q_PAD_ENET_RX_ER__ENET_1588_EVENT2_OUT,

  MX6Q_PAD_ENET_MDC__ENET_MDC,

  MX6Q_PAD_ENET_MDIO__ENET_MDIO,

  MX6Q_PAD_ENET_RXD0__ENET_RDATA_0,

  MX6Q_PAD_ENET_RXD1__ENET_RDATA_1,

  MX6Q_PAD_ENET_REF_CLK__ENET_TX_CLK,

  MX6Q_PAD_ENET_TXD0__ENET_TDATA_0,

  MX6Q_PAD_ENET_TXD1__ENET_TDATA_1,

  MX6Q_PAD_ENET_TX_EN__ENET_TX_EN,

  MX6Q_PAD_ENET_CRS_DV__ENET_RX_EN,

  MX6Q_PAD_RGMII_RX_CTL__ENET_RGMII_RX_CTL,

  MX6Q_PAD_RGMII_RXC__ENET_RGMII_RXC,

  MX6Q_PAD_RGMII_TX_CTL__ENET_ANATOP_ETHERNET_REF_OUT,

};

Anyone can help , thanks

Regards

Wilson

ラベル(1)
タグ(2)
0 件の賞賛
2 返答(返信)

806件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Are you still having issues to successfully connect? Which i.MX6 board are you using, a commercially available one or a custom board?

I would recommend checking your IP address (either if it’s static or you’re being assigned one, to make sure this is happening correctly). Open possibility is that you’re having either a conflict or that you’re not connected to the right network to be able to ping your server.

0 件の賞賛

806件の閲覧回数
wilsonlin
Contributor I

Yes,I check my enet_pads and it's work.

Thanks a lot.

0 件の賞賛