RT1170 EVK how to porting some filesystem on this board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1170 EVK how to porting some filesystem on this board

303件の閲覧回数
shawn_123
Contributor I

dear NXP engineer.

     i am using a RT1170 demo board in my project, and prepear to add function: using the board can to send some picture or UI related data to update the application running on it.  

my first question: i found the demo below driver folder "evkmimxrt1170\driver_examples\flexcan" i predict this is the can driver. is there any canoe project to be used can communicate with the EVK, for instance i send some picture data meant to update it to the board via can bus.  

my second question: is there any manul recommend to porting some filesystem to this board. which filesystem is opt to do this, give any advice. thanks a lot!

0 件の賞賛
1 返信

267件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @shawn_123 

I'm afraid there isn't a CAN project to update the board, since the iMXRT1170 bootloader only supports peripherals such as UART and USB.

On this link you will find the Getting Started for the iMXRT1170.

Best Regards, Miguel.

0 件の賞賛