RT1064 reflow and PCB layout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1064 reflow and PCB layout

969件の閲覧回数
barmic25
Contributor I

Hello, 

may i ask you to share files where reflow process (profile, temps) are indicated? 

Also, is there any file with recommended PCB layout, or only GERBER files from EVK? 

0 件の賞賛
3 返答(返信)

959件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

Could you please provide the complete part number of the RT that you are using so I can provide adequate information regarding the recommendations for the specific packaging type. 

For PCB recommendations, layout guidelines and other hardware considerations please use the following document:

Hardware Development Guidelines

Best Regards,

Sabina

 

0 件の賞賛

954件の閲覧回数
barmic25
Contributor I

Hello, 

 

full PN is 

MIMXRT1064DVL6A 
0 件の賞賛

947件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

 

Hope you are doing well. Thank you for providing the PN.

For the LFBGA package the following application notes will be useful:

AN10365

As well as the information in the following image:

nxf51209_0-1601058205640.png

 

Best Regards,

Sabina

 

0 件の賞賛