RT1061 debugging issue (JLink)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1061 debugging issue (JLink)

1,548件の閲覧回数
bjorns
Contributor III

Hello,

We are developing an application for NXP RT1061 (custom board) and are experiencing some issues when it comes to debugging. 

MCU: MIMXRT1061CVL5B
Flash: IS25LP032D
Debuger: JLink Plus


1. The JLink server seems to have problems halting the mcu after reset, when running and debugging from flash, hinting that we have faulty flash settings. (Flash configuration is appended at the end.)

This causes for example breakpoints in the beginning of main not to trigger. And possibly also other issues as described below.

Log from JLinkServer:
Received monitor command: reset
ResetTarget() start
Core did not halt on flash image verification. Assuming faulty flash settings.
Halting target manually.
ResetTarget() end

What causes this, do we have the wrong flash configuration?

2. We have no problem booting from the flash. However once a program is present in the flash the Jlink  Debugger is unable to reprogram the flash. Could be related to issue 1 since if we insert a delay in the beginning of main it works. We have some units which we at the moment are unable to recover because of this.

We suspect that configuring the MPU or something similar to this prevent JLink from uploading its "Ram code" but we have not been able to confirm this. We have however tried to disable the MPU using JLink commander but have not been successful. The FlexRam module has default configuration (128k DTC, 128K ITC, 256K OC).

JLink Commander Log:
J-Link>exec EnableEraseAllFlashBanks
J-Link>erase
Without any given address range, Erase Chip will be executed
Erasing device...
****** Error: Failed to prepare RAMCode using RAM
Error while determining flash info (Bank @ 0x60000000)
ERROR: Erase returned with error code -1.

3. Starting a debug session takes a long time.

The time from when the program has been written to flash/ram and the triggering of the first breakpoint in main is long sometimes more than a minute. This could for some reason be a related to the application size since we do not experience this issue when running nxp's example applications. Our application is around 400k. This happens both if we execute from ram and flash.

We are using McuXpresso.

What could be causing this? Anything we can do to improve the debugging experience.

Thanks
/Björn

 

 

Flash config:

const flexspi_nor_config_t qspiflash_config = {
.memConfig =
{
.tag = FLEXSPI_CFG_BLK_TAG,
.version = FLEXSPI_CFG_BLK_VERSION,
.readSampleClksrc=kFlexSPIReadSampleClk_LoopbackFromDqsPad,
.csHoldTime = 3u,
.csSetupTime = 3u,
.sflashPadType = kSerialFlash_4Pads,
.serialClkFreq = kFlexSpiSerialClk_100MHz,
.sflashA1Size = 4u * 1024u * 1024u,
.lookupTable =
{
// 0 Read LUTs
FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x18),
FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, 0x06, READ_SDR, FLEXSPI_4PAD, 0x04),
0,0,

// 1 Read Status
FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x81, READ_SDR, FLEXSPI_1PAD, 0x04),
0,0,0,

// 2 Reserved
0,0,0,0,

// 3 Write Enable
FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06, STOP, FLEXSPI_1PAD, 0),
0,0,0,

// 4 Reserved
0,0,0,0,

// 5 Erase Sector
FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xD7, RADDR_SDR, FLEXSPI_1PAD, 0x18),
0,0,0,

// 6 Reserved
0,0,0,0,

// 7 Reserved
0,0,0,0,

// 8 Reserved
0,0,0,0,

// 9 Page Program
FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x32, RADDR_SDR, FLEXSPI_1PAD, 0x18),
FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_4PAD, 0x04, STOP, FLEXSPI_1PAD, 0),
0,0,

// 10 Reserved
0,0,0,0,

// 11 Chip Erase
FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xC7, STOP, FLEXSPI_1PAD, 0),
0,0,0,

// 12 Reserved
0,0,0,0,
},
},
.pageSize = 256u,
.sectorSize = 4u * 1024u,
.blockSize = 64u * 1024u,
.isUniformBlockSize = false,
};

ラベル(1)
0 件の賞賛
9 返答(返信)

1,540件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, I'd like to know the ratio of the phenomenon that arises, second, I'd highly recommend you to use the tool to verify the FlexSPI connection, meanwhile, you'd better check the hardware board, especially, the power supply circuit.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

1,533件の閲覧回数
bjorns
Contributor III

Thanks for the answer.

What tool are you referring to?

The problems we are having is constant. It does not seem to change between runs.

I will as our hardware designer to dubble check the flash power supply circuit.

Thanks
/Björn

0 件の賞賛

1,520件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

 

Hi,
Thanks for your reply.
The tool is the NXP-MCUBootUtility, and I was wondering if you can update the schematic of the custom board.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

1,511件の閲覧回数
bjorns
Contributor III

Hello,

Thanks for your reply.

Is there any way to send you the schematics privately? 

When it comes to point 3 above, I have tried to debug using SEGGERS Ozone tool and it seems to be lightning fast with the same binary. It seems that mcuxpresso has some issue handling large projects or I have some configuration somewhere that is wrong. Is this a knonw issue?

Thanks
/Björn

0 件の賞賛

1,504件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Is there any way to send you the schematics privately?
-- Maybe you can send a download link via the private message
1) Is this a knonw issue?
-- No.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

1,490件の閲覧回数
bjorns
Contributor III

Hello,

I have got OK to post parts of the schematic. Let me know if this is enough.

Thanks for your help.
/Björn


0 件の賞賛

1,488件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
Actually, I've not found something wrong after checking the above picture, further, the Flash configuration is good.
Did you already use the NXP-MCUBootUtility for testing? Moreover, does it encounter a similar issue when debugging the demos from the SDK library for the RT106x?
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

1,483件の閲覧回数
bjorns
Contributor III

I have been trying to get the NXP-MCUBoot utility to work but it refuses to connect over lpuart1. What test can it perform? I cant find anything about flash testing in the description of the tool.

Yes, we see the same issues when debugging the the sdk examples.

Thanks
/Björn

0 件の賞賛

1,470件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) What test can it perform? I can't find anything about flash testing in the description of the tool.
-- During building connection with the NXP-MCUBoot utility, it will configure the external memory device, if it fails, it illustrates there's something wrong with the hardware.
Further, you can use either LPUART1 (GPIO_AD_B0_12 and GPIO_AD_B0_13)or USB OTG1 to connect the tool.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛