RT1021 QSPI NOR flash support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1021 QSPI NOR flash support?

Jump to solution
1,081 Views
StephenYeh
Contributor III

Hi Sir,
If the QSPI NOR flash max speed will be 133Mhz. would the RT1021 can support or not.

W is the RT1021 max. speed for QSPI flash?

0 Kudos
Reply
1 Solution
1,076 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @StephenYeh ,

    Please check the RT1021 datasheet, you will be more clear:

kerryzhou_0-1646975678935.png

So, it can support 133Mhz.

Best Regards,

Kerry

 

View solution in original post

0 Kudos
Reply
5 Replies
1,064 Views
StephenYeh
Contributor III

Hi Kerry

Thank for your reply.

Could you share all the cmd list that RT1021 require?

0 Kudos
Reply
1,063 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @StephenYeh ,

   About the used command, you can check the SDK code:

SDK_2_11_0_EVK-MIMXRT1020\boards\evkmimxrt1020\driver_examples\flexspi\nor\polling_transfer

const uint32_t customLUT[CUSTOM_LUT_LENGTH] = {
    /* Normal read mode -SDR */
    /* Normal read mode -SDR */
    [4 * NOR_CMD_LUT_SEQ_IDX_READ_NORMAL] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x03, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
    [4 * NOR_CMD_LUT_SEQ_IDX_READ_NORMAL + 1] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),

    /* Fast read mode - SDR */
    [4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x0B, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
    [4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST + 1] = FLEXSPI_LUT_SEQ(
        kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_1PAD, 0x08, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04),

    /* Fast read quad mode - SDR */
    [4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0xEB, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_4PAD, 0x18),
    [4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD + 1] = FLEXSPI_LUT_SEQ(
        kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_4PAD, 0x06, kFLEXSPI_Command_READ_SDR, kFLEXSPI_4PAD, 0x04),

    /* Read extend parameters */
    [4 * NOR_CMD_LUT_SEQ_IDX_READSTATUS] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x81, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04),

    /* Write Enable */
    [4 * NOR_CMD_LUT_SEQ_IDX_WRITEENABLE] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x06, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),

    /* Erase Sector  */
    [4 * NOR_CMD_LUT_SEQ_IDX_ERASESECTOR] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0xD7, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),

    /* Page Program - single mode */
    [4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_SINGLE] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x02, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
    [4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_SINGLE + 1] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),

    /* Page Program - quad mode */
    [4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_QUAD] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x32, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
    [4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_QUAD + 1] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_4PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),

    /* Read ID */
    [4 * NOR_CMD_LUT_SEQ_IDX_READID] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x9F, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04),

    /* Enable Quad mode */
    [4 * NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x01, kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04),

    /* Enter QPI mode */
    [4 * NOR_CMD_LUT_SEQ_IDX_ENTERQPI] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x35, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),

    /* Exit QPI mode */
    [4 * NOR_CMD_LUT_SEQ_IDX_EXITQPI] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_4PAD, 0xF5, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),

    /* Read status register */
    [4 * NOR_CMD_LUT_SEQ_IDX_READSTATUSREG] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x05, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04),

    /* Erase whole chip */
    [4 * NOR_CMD_LUT_SEQ_IDX_ERASECHIP] =
        FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0xC7, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
};

 

You can find all the related command.

Eg, normal read:0X03, but in the app code, normally use fast read: 0XEB.

Wish it helps you!

Best Regards,

Kerry

 

0 Kudos
Reply
1,069 Views
StephenYeh
Contributor III

Hi Kerry

Thanks

 

If we want to cut in the 2'ed part.

GD25Q64E to replace  GD25Q64C

and MX25L6433F to replace MX25L64356

We compare the command list as below.

How to check that 2'ed part could support RT1021 boot? Would you share more detail for us?

 

MXIC_NorFlash.JPGGD_NorFlash.JPG

0 Kudos
Reply
1,068 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @StephenYeh ,

  I checked your list, in fact, the used command still the same, so you can use your replaced QSPI flash chip.

  Best Regards,

Kerry

0 Kudos
Reply
1,077 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @StephenYeh ,

    Please check the RT1021 datasheet, you will be more clear:

kerryzhou_0-1646975678935.png

So, it can support 133Mhz.

Best Regards,

Kerry

 

0 Kudos
Reply