RT1021 MCUXpresso Whether the compilation environment is faulty?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1021 MCUXpresso Whether the compilation environment is faulty?

Jump to solution
3,879 Views
jarman_zhou
Contributor I

MCUXpresso IDE v11.5.1 Compile SAI exception,See the code description

1.Loop assignment and individual assignment

1.png

2.Adds a print, but does not execute it

2.png

 

SDK_2_11_0_EVK-MIMXRT1020

0 Kudos
1 Solution
3,560 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @jarman_zhou ,

  我刚才直接跑了下你的代码,没有任何修改的情况下,是能听到声音采集传输回来的,就是有点杂音,没有完全变形。

  然后我看了下你的代码,算了下你的几个大数组情况,已经很大了。如果是DTCM 配的0X8000,肯定是不够的。

  情况这样:

16ms一次传输的数组: 6144byte, buffer定义了4个,就是6144*4=0X6000。

然后你又定义了其他几个整形数组:

int pTemp[BUFFER_SIZE/sizeof(int)] = {0};
int pMic[BUFFER_SIZE/sizeof(int)] = {0};
int pSendXfer[BUFFER_SIZE/sizeof(int)] = {0};

算下:6144*3=0X4800

总共:0X4800+6000=0XA800。

所以如果你定义0X8000,内存肯定是超了。

但是你想,我用SDRAM了,实际上SDRAM用做stack,还需要注意cache的情况,使用起来没那么顺畅。

所以,我建议你一个buffer可以做小点,就像你之前说的:如果将SIGLE_SAMPLE 改成8ms或者更小一点就正常。

这样耗费的stack会小一些,只是处理的勤快一点而已。

不知道,你那边是否能接收以代码换内存空间的方法?

实在不行,你把stack放大, heap减小点。stack可不能只是差不多0XA800,还得大,因为函数进出,中断进出,变量都得用,heap因为没有用malloc,我认为可以小。

RT1021的DTCM默认64K, 实在不够,你flexRAM重新分区,给DTCM搞大,OCRAM 搞小。

kerryzhou_0-1685694636674.png

我算算,也是足够用了。可以把DTCM做到128K。

关于重新分区,可以参考我这个文章:

https://www.nxpic.org.cn/module/forum/thread-619452-1-1.html

我看你现在的map文件:

kerryzhou_1-1685695112752.png

大小其实也是不行的。

所以目前两个建议:

1. 减小buffersize,我觉得也没必要一次处理时间太长,8ms,4ms其实都可以。

2.重新分区flexRAM, 把DTCM做到128K,然后stack size拉大,大过你所有的buffer空间,并且再加0x1000给其他耗用内存的用。

你那边试试看,如果还有问题,我们继续交流和测试!

Best Regards,

Kerry

 

 

 

 

 

 

 

View solution in original post

0 Kudos
28 Replies
3,399 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @jarman_zhou ,

  I test your project on my MIMXRT1020-EVK, it meet the assert issue:

kerryzhou_0-1685003896790.png

Do you have this issue?

Best Regards,

Kerry

 

0 Kudos
3,393 Views
jarman_zhou
Contributor I

Hi @kerryzhou

If my project runs incorrectly on your board, you can try to import the project directly from your local SDK and modify it against the project I provided.

Best Regards,

Jarman

0 Kudos
3,390 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @jarman_zhou ,

   Ok, I can test it based on the SDK directly.

   One question, how do you know the data is incorrect, as you mentioned the sound is wrong with your related code, do you play the music?

 

Best Regards,

Kerry

0 Kudos
3,388 Views
jarman_zhou
Contributor I

Hi @kerryzhou

This project is a recording - play mode, the microphone on the board can be given to the headphone output. I could hear my voice passing through the microphone

Best Regards,

Jarman

0 Kudos
3,346 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @jarman_zhou ,

  我们可以直接用中文交流。

   我先说下对你问题的理解,目前你是发现在DMA传输的过程重,添加了一些其他的操作,比如:

#if 1
            memcpy(pTemp, xfer.data, BUFFER_SIZE);
 
            for(int i=0; i<64; i++)
{
for(int j=0; j<2; j++)
{
pMic[j*64 + i] = pTemp[2*i+j];
}
}
 
            for(int i=0; i<64; i++)
{
for(int j=0; j<2; j++)
{
//pMic[j*64 + i] = pMic[j*64 + i]>>2;//(1) Shift one bit to the right
pMic[j*64 + i] = pMic[j*64 + i]<<1;//(2) Shift one bit to the left
pMic[j*64 + i] = pMic[j*64 + i];
}
}
 
            for(int i=0; i<64; i++)
{
for(int j=0; j<2; j++)
{
pTemp[2*i+j] = pMic[j*64 + i];
}
}
 
            memcpy(xfer.data, (void *)pTemp, BUFFER_SIZE);
#endif
实际上也不影响真实的SAI MIC到播放数据,只是你发现一旦你对数据处理了,然后听到的声音就不对了,是吗?
你添加相关数据处理代码,也是为了麦的数据处理,但是不希望影响到同步传输播放这层,是这个道理吧?
如果是这个情况,通常是会用多buffer去做DMA传输,避开处理对传输buffer的影响。
请帮我确认下,我对你问题的理解是否有偏差,这样便于我测试,谢谢理解。
 
Best Regards,
Kerry
0 Kudos
3,318 Views
jarman_zhou
Contributor I

Hi @kerryzhou

是的,你理解的是对的,因为我的需求每次处理4通道/4ms的TDM,总长度是3072,这样只要我对数据任何1bit进行改变,声音都会不正常。但是我尝试改变这个长度,比如请求2通道,或者请求1ms就不会有问题,所以我判断是请求的长度影响到了程序的正常运行。

Best Regards,

Jarman

0 Kudos
3,304 Views
kerryzhou
NXP TechSupport
NXP TechSupport

你现在是跑下面这段main出问题吗?我看你代码里两个main:

	int main(void)
	{
	    sai_transfer_t xfer, send_xfer;
	    edma_config_t dmaConfig = {0};
	    sai_transceiver_t saiConfig;

	    BOARD_ConfigMPU();
	    BOARD_InitBootPins();
	    BOARD_InitBootClocks();
	    CLOCK_InitAudioPll(&audioPllConfig);
	    BOARD_InitDebugConsole();

	    /*Clock setting for LPI2C*/
	    CLOCK_SetMux(kCLOCK_Lpi2cMux, DEMO_LPI2C_CLOCK_SOURCE_SELECT);
	    CLOCK_SetDiv(kCLOCK_Lpi2cDiv, DEMO_LPI2C_CLOCK_SOURCE_DIVIDER);

	    /*Clock setting for SAI1*/
	    CLOCK_SetMux(kCLOCK_Sai1Mux, DEMO_SAI1_CLOCK_SOURCE_SELECT);
	    CLOCK_SetDiv(kCLOCK_Sai1PreDiv, DEMO_SAI1_CLOCK_SOURCE_PRE_DIVIDER);
	    CLOCK_SetDiv(kCLOCK_Sai1Div, DEMO_SAI1_CLOCK_SOURCE_DIVIDER);

	    /*Enable MCLK clock*/
	    BOARD_EnableSaiMclkOutput(true);

	    /* Init DMAMUX */
	    DMAMUX_Init(DEMO_DMAMUX);
	    DMAMUX_SetSource(DEMO_DMAMUX, DEMO_TX_EDMA_CHANNEL, (uint8_t)DEMO_SAI_TX_SOURCE);
	    DMAMUX_EnableChannel(DEMO_DMAMUX, DEMO_TX_EDMA_CHANNEL);
	    DMAMUX_SetSource(DEMO_DMAMUX, DEMO_RX_EDMA_CHANNEL, (uint8_t)DEMO_SAI_RX_SOURCE);
	    DMAMUX_EnableChannel(DEMO_DMAMUX, DEMO_RX_EDMA_CHANNEL);

	    PRINTF("SAI example started!\n\r");

	    /* Init DMA and create handle for DMA */
	    EDMA_GetDefaultConfig(&dmaConfig);
	    EDMA_Init(DEMO_DMA, &dmaConfig);
	    EDMA_CreateHandle(&dmaTxHandle, DEMO_DMA, DEMO_TX_EDMA_CHANNEL);
	    EDMA_CreateHandle(&dmaRxHandle, DEMO_DMA, DEMO_RX_EDMA_CHANNEL);
	#if defined(FSL_FEATURE_EDMA_HAS_CHANNEL_MUX) && FSL_FEATURE_EDMA_HAS_CHANNEL_MUX
	    EDMA_SetChannelMux(DEMO_DMA, DEMO_TX_EDMA_CHANNEL, DEMO_SAI_TX_EDMA_CHANNEL);
	    EDMA_SetChannelMux(DEMO_DMA, DEMO_RX_EDMA_CHANNEL, DEMO_SAI_RX_EDMA_CHANNEL);
	#endif

	    /* SAI init */
	    SAI_Init(DEMO_SAI);

	    SAI_TransferTxCreateHandleEDMA(DEMO_SAI, &txHandle, tx_callback, NULL, &dmaTxHandle);
	    SAI_TransferRxCreateHandleEDMA(DEMO_SAI, &rxHandle, rx_callback, NULL, &dmaRxHandle);

	    /* I2S mode configurations */
	    //SAI_GetClassicI2SConfig(&saiConfig, DEMO_AUDIO_BIT_WIDTH, kSAI_Stereo, 1U << DEMO_SAI_CHANNEL);
	    SAI_GetTDMConfig(&saiConfig, kSAI_FrameSyncLenOneBitClk, DEMO_AUDIO_BIT_WIDTH, DEMO_AUDIO_DATA_CHANNEL, 1U << DEMO_SAI_CHANNEL);
	    saiConfig.frameSync.frameSyncEarly = true;
	    saiConfig.syncMode              = DEMO_SAI_TX_SYNC_MODE;
	    //saiConfig.bitClock.bclkPolarity = DEMO_SAI_TX_BIT_CLOCK_POLARITY;
	    //saiConfig.masterSlave           = DEMO_SAI_MASTER_SLAVE;
	    SAI_TransferTxSetConfigEDMA(DEMO_SAI, &txHandle, &saiConfig);
	    saiConfig.syncMode = DEMO_SAI_RX_SYNC_MODE;
	    SAI_TransferRxSetConfigEDMA(DEMO_SAI, &rxHandle, &saiConfig);

	    /* set bit clock divider */
	    SAI_TxSetBitClockRate(DEMO_SAI, DEMO_AUDIO_MASTER_CLOCK, DEMO_AUDIO_SAMPLE_RATE, DEMO_AUDIO_BIT_WIDTH,
	                          DEMO_AUDIO_DATA_CHANNEL);
	    SAI_RxSetBitClockRate(DEMO_SAI, DEMO_AUDIO_MASTER_CLOCK, DEMO_AUDIO_SAMPLE_RATE, DEMO_AUDIO_BIT_WIDTH,
	                          DEMO_AUDIO_DATA_CHANNEL);

	    /* master clock configurations */
	    BOARD_MASTER_CLOCK_CONFIG();

	    /* Use default setting to init codec */
	    if (CODEC_Init(&codecHandle, &boardCodecConfig) != kStatus_Success)
	    {
	        assert(false);
	    }
	    if (CODEC_SetVolume(&codecHandle, kCODEC_PlayChannelHeadphoneLeft | kCODEC_PlayChannelHeadphoneRight,
	                        DEMO_CODEC_VOLUME) != kStatus_Success)
	    {
	        assert(false);
	    }

	    int pTemp[BUFFER_SIZE/sizeof(int)] = {0};
	    int pMic[BUFFER_SIZE/sizeof(int)] = {0};
	    int pSendXfer[BUFFER_SIZE/sizeof(int)] = {0};

	    send_xfer.data     = pSendXfer;
	    send_xfer.dataSize = BUFFER_SIZE;
	    while (1)
	    {
	        if (rx_callback_finished)
	        {
	        	rx_callback_finished = false;
	        	//PRINTF("emptyBlock1=%d\r\n",emptyBlock);
	        	xfer.data     = Buffer + rx_index * BUFFER_SIZE;
	        	xfer.dataSize = BUFFER_SIZE;
	            if (kStatus_Success == SAI_TransferReceiveEDMA(DEMO_SAI, &rxHandle, &xfer))
	            {
	            	rx_index++;
	            }
	            if (rx_index == BUFFER_NUMBER)
	            {
	                rx_index = 0U;
	            }
	        }
	        if (tx_callback_finished)
	        {
	        	tx_callback_finished = false;
	        	xfer.data     = Buffer + tx_index * BUFFER_SIZE;
	        	xfer.dataSize = BUFFER_SIZE;
#if 1
				memcpy(pTemp, xfer.data, BUFFER_SIZE);

				for(int i=0; i<SIGLE_SAMPLE; i++)
				{
					for(int j=0; j<DEMO_AUDIO_DATA_CHANNEL; j++)
					{
						pMic[j*SIGLE_SAMPLE + i] = pTemp[DEMO_AUDIO_DATA_CHANNEL*i+j];
					}
				}

				for(int i=0; i<SIGLE_SAMPLE; i++)
				{
					for(int j=0; j<DEMO_AUDIO_DATA_CHANNEL; j++)
					{
						//pMic[j*SIGLE_SAMPLE + i] = pMic[j*SIGLE_SAMPLE + i]<<1;//(1) Shift one bit to the right
						//pMic[j*64 + i] = pMic[j*64 + i]<<1;//(2) Shift one bit to the left
						//pMic[j*64 + i] = pMic[j*64 + i];
					}
				}

				for(int i=0; i<SIGLE_SAMPLE; i++)
				{
					for(int j=0; j<DEMO_AUDIO_DATA_CHANNEL; j++)
					{
						pTemp[DEMO_AUDIO_DATA_CHANNEL*i+j] = pMic[j*SIGLE_SAMPLE + i];
					}
				}

				memcpy(send_xfer.data, (void *)pTemp, BUFFER_SIZE);
	#endif
	            if (kStatus_Success == SAI_TransferSendEDMA(DEMO_SAI, &txHandle, &send_xfer))
	            {
	                tx_index++;
	            }
	            if (tx_index == BUFFER_NUMBER)
	            {
	                tx_index = 0U;
	            }
	        }
	    }

	}

 

最关键是这个代码加了出问题吗?

#if 1
memcpy(pTemp, xfer.data, BUFFER_SIZE);
 
for(int i=0; i<SIGLE_SAMPLE; i++)
{
for(int j=0; j<DEMO_AUDIO_DATA_CHANNEL; j++)
{
pMic[j*SIGLE_SAMPLE + i] = pTemp[DEMO_AUDIO_DATA_CHANNEL*i+j];
}
}
 
for(int i=0; i<SIGLE_SAMPLE; i++)
{
for(int j=0; j<DEMO_AUDIO_DATA_CHANNEL; j++)
{
//pMic[j*SIGLE_SAMPLE + i] = pMic[j*SIGLE_SAMPLE + i]<<1;//(1) Shift one bit to the right
//pMic[j*64 + i] = pMic[j*64 + i]<<1;//(2) Shift one bit to the left
//pMic[j*64 + i] = pMic[j*64 + i];
}
}
 
for(int i=0; i<SIGLE_SAMPLE; i++)
{
for(int j=0; j<DEMO_AUDIO_DATA_CHANNEL; j++)
{
pTemp[DEMO_AUDIO_DATA_CHANNEL*i+j] = pMic[j*SIGLE_SAMPLE + i];
}
}
 
memcpy(send_xfer.data, (void *)pTemp, BUFFER_SIZE);
#endif
如果不处理,就可以正常,对吗?
我这边的MIMXRT1020-EVK 板子的codec出了问题,这也是为什么跑你代码进入assert,我要再找个板子测下。
看你的问题情况,应该还是和软件代码的处理有关,因为我们这边有处理8通道的SAI数据都能正常。
你现在的数据处理是想实现什么功能?音频数据变换之后,看上去已经改变了,如何保证播放的数据和采集数据的一致?
 
Best Regards,
Kerry

 

 

0 Kudos
3,299 Views
jarman_zhou
Contributor I

Hi @kerryzhou

这个程序我是特意加大了EDMA的请求数据的大小

#define SIGLE_SAMPLE (DEMO_AUDIO_SAMPLE_RATE*16/1000)//16MS
#define BUFFER_SIZE (SIGLE_SAMPLE*DEMO_AUDIO_DATA_CHANNEL*sizeof(int))

这样经过处理之后就会有问题,如果将SIGLE_SAMPLE 改成8ms或者更小一点就正常。

处理数据,我只是简单的取出了每个通道的数据进行移位操作,相当于改变音量大小,并不会对数据正确性造成影响。后面音频正常后我会加入滤波器/EQ等算法。算法会处理多个通道的数据。

以上是EVK板上的情况。

事实上我调试自己的板子,只是采集数据直接给到播放时没有问题,但是一旦我加了如下的代码就会出现问题

#if 1
memcpy(pTemp, xfer.data, BUFFER_SIZE);
 
for(int i=0; i<SIGLE_SAMPLE; i++)
{
for(int j=0; j<DEMO_AUDIO_DATA_CHANNEL; j++)
{
pMic[j*SIGLE_SAMPLE + i] = pTemp[DEMO_AUDIO_DATA_CHANNEL*i+j];
}
}
 
for(int i=0; i<SIGLE_SAMPLE; i++)
{
for(int j=0; j<DEMO_AUDIO_DATA_CHANNEL; j++)
{
pMic[j*SIGLE_SAMPLE + i] = pMic[j*SIGLE_SAMPLE + i]>>1;
}
}
//PRINTF("TEST\r\n");//比如这里加一句PRINTF,但是该条语句是屏蔽的
for(int i=0; i<SIGLE_SAMPLE; i++)
{
for(int j=0; j<DEMO_AUDIO_DATA_CHANNEL; j++)
{
pTemp[DEMO_AUDIO_DATA_CHANNEL*i+j] = pMic[j*SIGLE_SAMPLE + i];
}
}
 
memcpy(send_xfer.data, (void *)pTemp, BUFFER_SIZE);
#endif
 
但是我修改xfer.dataSize的大小就会正常,感觉跟内存有关,比如我加了一个PRINTF的打印,并且屏蔽掉它,也会影响到音频
0 Kudos
3,287 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @jarman_zhou ,

   我看下来也是和内存有关,所以你看看把工程的stack size, heap size放大看看,有没有用?

    毕竟你的数组和你的长度直接有关,所以我想你把stack, heap都改大,在工程属性里面修改,这样linker file也会自动修改。

Best Regards,

Kerry

0 Kudos
3,283 Views
jarman_zhou
Contributor I

Hi @kerryzhou

我尝试过修改stack和heap到最大,也是没有改善的。我还修改过编译器的优化等级,都没有解决。

0 Kudos
3,280 Views
kerryzhou
NXP TechSupport
NXP TechSupport

你目前stack heap size是多大?

你修改到最大是多大?

 

0 Kudos
3,276 Views
jarman_zhou
Contributor I

Hi @kerryzhou

我现在使用的是SDRAM,堆栈设置的是8M.

1.png

我也使用过DTC,堆栈配置32k

2.png

0 Kudos
3,561 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @jarman_zhou ,

  我刚才直接跑了下你的代码,没有任何修改的情况下,是能听到声音采集传输回来的,就是有点杂音,没有完全变形。

  然后我看了下你的代码,算了下你的几个大数组情况,已经很大了。如果是DTCM 配的0X8000,肯定是不够的。

  情况这样:

16ms一次传输的数组: 6144byte, buffer定义了4个,就是6144*4=0X6000。

然后你又定义了其他几个整形数组:

int pTemp[BUFFER_SIZE/sizeof(int)] = {0};
int pMic[BUFFER_SIZE/sizeof(int)] = {0};
int pSendXfer[BUFFER_SIZE/sizeof(int)] = {0};

算下:6144*3=0X4800

总共:0X4800+6000=0XA800。

所以如果你定义0X8000,内存肯定是超了。

但是你想,我用SDRAM了,实际上SDRAM用做stack,还需要注意cache的情况,使用起来没那么顺畅。

所以,我建议你一个buffer可以做小点,就像你之前说的:如果将SIGLE_SAMPLE 改成8ms或者更小一点就正常。

这样耗费的stack会小一些,只是处理的勤快一点而已。

不知道,你那边是否能接收以代码换内存空间的方法?

实在不行,你把stack放大, heap减小点。stack可不能只是差不多0XA800,还得大,因为函数进出,中断进出,变量都得用,heap因为没有用malloc,我认为可以小。

RT1021的DTCM默认64K, 实在不够,你flexRAM重新分区,给DTCM搞大,OCRAM 搞小。

kerryzhou_0-1685694636674.png

我算算,也是足够用了。可以把DTCM做到128K。

关于重新分区,可以参考我这个文章:

https://www.nxpic.org.cn/module/forum/thread-619452-1-1.html

我看你现在的map文件:

kerryzhou_1-1685695112752.png

大小其实也是不行的。

所以目前两个建议:

1. 减小buffersize,我觉得也没必要一次处理时间太长,8ms,4ms其实都可以。

2.重新分区flexRAM, 把DTCM做到128K,然后stack size拉大,大过你所有的buffer空间,并且再加0x1000给其他耗用内存的用。

你那边试试看,如果还有问题,我们继续交流和测试!

Best Regards,

Kerry

 

 

 

 

 

 

 

0 Kudos
3,060 Views
jarman_zhou
Contributor I

Hi @kerryzhou

我修改DTCM的大小为128k后,下载进板子可以运行,此时stack大小为默认的4k。

但是只要我修改stack的大小超过了64k,程序就不能运行,感觉还是没有修改成功。

1.png2.png3.png

0 Kudos
3,016 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @jarman_zhou ,

   超过64K跑不起来,说明还是有问题,你是debug的吗?如果debug ,并且使用的是CMSIS DAP, 你要修改scp。

  你这样,你打印下flexRAM的配置相关寄存器,看看是否改成功了。

   另外,你把你最新的这个代码,就是超过64k的这个工程发我,我给你看看。

 

Best Regards,

kerry

0 Kudos
2,981 Views
jarman_zhou
Contributor I

Hi @kerryzhou

昨天我修改后可以跑起来了,之前可能是哪个地方没有配置正确,程序运行了但是音频还是和之前一样有失真。修改见附件

另外我还有一个问题请教,sai是否能和http一起使用,我现在把两个功能都打开,发现当有http请求的时候会导致音频数据出现错误。

0 Kudos
2,976 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @jarman_zhou ,

     我可以肯定,SAI可以和http一起跑,因为我之前做过一个天气预报,就是http+音频的,你可以看看我的文章:

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/The-RT-speech-recognition-system-based-on-VIT-to...

 

    关于代码debug,您可以帮我重新建一个帖子吗?因为这个问题时间太长了,超过4周我需要一直解释,所以麻烦您帮我重新建一个问题,我找个时间给你debug。

Best Regards,

Kerry

0 Kudos
3,130 Views
jarman_zhou
Contributor I

Hi @kerryzhou

我尝试按照你提供的方法修改DTC的大小,但是没有成功

1.找到要修改的GRP17的值

1.png

2.修改startup_mimxrt1021.c的代码,但是我不太明白TCM_CTRL,GRP16,GRP14这几个寄存器的含义

2.png

3.修改Memory大小

3.png

4.编译之后使用MCUBootUtility下载到板子,但是没有运行,所以我没有写.scp文件

请帮我检查一下上面步骤是否有问题,谢谢

0 Kudos
3,226 Views
jarman_zhou
Contributor I

Hi @kerryzhou

我现在的项目用的是SDRAM,实际上我请求的数据数据长度是48*4*4ch*4ms=3072,这个长度对于SDRAM应该是没问题。可能项目中还有其他功能模块要加,估计是要使用到SDRAM。你提到的要考虑的cache,这个可以优化吗?使用SDRAM对音频的性能会不会有影响

如果使用DTC,把空间改大,会有cache这个因素影响吗?

 

0 Kudos
3,222 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi@jarman_zhou 

   你好!

    SDRAM使用没有问题,不过对于stack这些,我建议还是用内部的比较好点。

    DTCM,ITCM不会受cache影响,而且速度快。 SDRAM是从SEMC接口走的,没有内部的快。

   你还要做数据处理,而且DTCM也够用,我建议你用DTCM。

kerryzhou_0-1685698144640.png

这个图比较清楚,你看到内核和DTCM, ITCM直接交互。但是OCRAM, SDRAM要走interconnect bus fabrics.用不好,会有冲突。

不过,用SDRAM了,你就把相关stack放到noncache区域中去,实在不行,关闭cache,具体你可以查看我们的AN12042。

你先使用DTCM改大看看,如果还是有问题,你更新后的工程再发我,我再复现你的问题。

Best Regards,

Kerry

 

 

0 Kudos