RT1021 Failed to erase NOR FALSH after replacement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1021 Failed to erase NOR FALSH after replacement

278 Views
bobhi009
Contributor I

The NOR FLASH of 32MB on the evk board can be erased properly. However, after the NOR FLASH of 256MB (MX25L25645GM2I-10G) is replaced, the flexspi_nor_flash_erase_sector does not return any error. However, the data in the sector cannot be erased (can read and write data normally).

Tags (1)
0 Kudos
Reply
1 Reply

267 Views
jay_heng
NXP Employee
NXP Employee

It is IS25LP064A-JBLE (8MB) in NXP MIMXRT1020-EVK board, SDK flexspi example is mainly for this flash.

If you use different flash, you may need to check Flash Data sheet and modify flexspi example (focus on customLUT) if necessary.

I have one unit test project for your reference:

https://github.com/JayHeng/RT-MFB/tree/main/boards/mimxrt/mfb_fw/src

0 Kudos
Reply