I am posting this here for everyone to know
Anybody can tell us the ROOT password for this BSP ?
Linux Binary Demo Files 2011.01.
Size (K): 946416 Format: gz Rev #: 2011.01 Modified: 3/9/2011
and maybe confirm the same for this new BSP at the same time.
Linux Binary Demo Files 2011.03 Release.
Size (K): 227202 Format: gz Rev #: 2011.03 Modified: 4/15/2011
Thanks
François Anderson
@Claude:
SD-Card with my i.MX53 QSB is having the same number as yours (L2.6.35_11.01ER_77347A). I think you need to enter lucid only. If I have just installed updates on my QSB and it works fine.
Regards
Wajid
Just my 2-cents worth...
Ubantu, by default, does not sets up root user when setting up. So if you tried to login root, naturally it will reject, independent of password you use.
You just use sudo to perform root priviledged operation. I was able to login lucid / lucid for both LCD and the console.
Since I deal with a few other systems (and I am not sitting in front of 53QSB right now) perhaps I am confused but I thought sudo (root priviledged command) with password lucid worked.
I haven't put the Freescale Linux BSP on the board, but on previous BSPs for other parts, the root password has been usually blank, so I would try that.
The lucid username/password combination is for the Ubuntu image. I'm not sure what the root password there is, but the lucid user has full sudo access, so you can do a sudo passwd root and change it.