Hello everyone,
We have a custom hardware with i.MX6 Quad CPU. we would like to use its RMII interface to communicate with KSZ8051RNL PHY.Configuration, detection and communication seem to be right, but we see a very high number of broken network packages when copying data via scp from PC to custom hardware via PHY Ethernet. Interestingly, the reverse direction does not have this problem.I mean to say TX(FEC ->PHY->HOST) communication is fine.
Here is the statistic.
cat /sys/custom/net/eth0/statistics/*
collisions 0
multicast 0
rx_bytes 4338780
rx_compressed 0
rx_crc_errors 504
rx_dropped 0
rx_errors 1229
rx_fifo_errors 0
rx_frame_errors 725
rx_length_errors 0
rx_missed_errors 0
rx_over_errors 0
rx_packets 8236
tx_aborted_errors 0
tx_bytes 6200152
tx_carrier_errors 0
tx_compressed 0
tx_dropped 0
tx_errors 0
tx_fifo_errors 0
tx_heartbeat_errors 0
tx_packets 8719
tx_window_errors 0
The system uses GPIO_16 pin to generate the reference clock.we have also enabled SION bit in imx6q-pinfunch.h
#define MX6QDL_PAD_GPIO_16__ENET_REF_CLK_RMII 0x248 0x618 0x83c 0x12 0x1
Device Tree:
pinctrl_enet: enetgrp {
fsl,pins = <
MX6QDL_PAD_KEY_COL3__ENET_CRS 0x1b0b0
MX6QDL_PAD_ENET_MDIO__ENET_MDIO 0x1b0b0
MX6QDL_PAD_ENET_MDC__ENET_MDC 0x1b0b0
MX6QDL_PAD_GPIO_16__ENET_REF_CLK_RMII 0x1b0b0
MX6QDL_PAD_ENET_RXD0__ENET_RX_DATA0 0x1b0b0
MX6QDL_PAD_ENET_RXD1__ENET_RX_DATA1 0x1b0b0
MX6QDL_PAD_ENET_CRS_DV__ENET_RX_EN 0x1b0b0
MX6QDL_PAD_ENET_RX_ER__ENET_RX_ER 0x1b0b0
MX6QDL_PAD_ENET_TXD0__ENET_TX_DATA0 0x1b0b0
MX6QDL_PAD_ENET_TXD1__ENET_TX_DATA1 0x1b0b0
MX6QDL_PAD_ENET_TX_EN__ENET_TX_EN 0x1b0b0
MX6QDL_PAD_GPIO_19__ENET_TX_ER 0x1b0b0
MX6QDL_PAD_EIM_DA9__GPIO3_IO09 0x0b0b0
MX6QDL_PAD_EIM_DA8__GPIO3_IO08 0x0b0b0
>;
};
&fec { /* KSZ8051RNLU RMII interface */
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_enet>;
phy-mode = "rmii";
phy-reset-gpios = <&gpio3 9 0>; /* RMII_nRST GPIO3_I009 */
#if 0
interrupt-parent = <&gpio3>; /* RMII Phy Interrupt GPIO3_IOO8 */
interrupts = <8 IRQ_TYPE_LEVEL_LOW>;
#endif
status = "okay";
};
Tested software versions:
Linux nitrogen6x 4.1.37
I would like to understand following things.
1: WHY only issue in RX Channel.
2: We could see CRC and Frame error. what could be the reason.
Any help would be appreciated.
已解决! 转到解答。
Look into this thread, maybe it helps with your problem:
https://community.nxp.com/thread/389902
Regards
Hi sanjeev
one can try with nxp bsp releases described on
i.MX 6 / i.MX 7 Series Software and Development Tool|NXP
Linux nitrogen6x 4.1.37 is not supported by nxp, it is developed by boundary
devices and issue may posted on meta-fsl-arm mailing list, so that someone
familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
we tried on 4.1.15 kernel version with NXP BSP also but we found same result.we didn't find difference in PHY driver and Ethernet controller driver(fec). It seems configuration or clock issue.
I could find https://community.nxp.com/thread/448768 issue which is similar to us. Please provide help in this context.
Regards
Sanjeev Sharma
Hi,
we can't reproduced on nxp reference board because we can't use KSZ8051RNL PHY on nxp reference board. Do you see some configuration issue in these type of Errors ?
Regards
Sanjeev Sharma