RMII connections - SX and LAN8720

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RMII connections - SX and LAN8720

跳至解决方案
1,204 次查看
Richard1z
Contributor II

I want to use a LAN8720 (RMII) with the iMX6SX.

The IMX6SXHDG does not cover the Ethernet Interface at all.

The SX Reference Manual covers it very badly.

If anyone has got the combination of LAN8720 + SX working correctly, I be obliged if they could review my schematics below or share theirs.

(My biggest cause for concern is the generation of the REF_CLK  - as there seems to continual confusion about this.)

pastedImage_0.png

pastedImage_1.png

pastedImage_2.png

标签 (1)
0 项奖励
1 解答
806 次查看
Richard1z
Contributor II

Hi Weidong.

thank you very much for this helpful information !

R

在原帖中查看解决方案

0 项奖励
2 回复数
806 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Richard,

See following , please!

(1) ENET1_REF_CLK_25MHz( PAD: NET1_RX_CLK or GPIO1_IO03)

---NET1_RX_CLK or GPIO1_IO03 pin can output 25MHz clock for LAN8720A, not PAD ENET1_TX_CLK, see page 1028 of reference manual.

---About Reference Clock input for CPU

Pad ENET1_TX_CLK can be used to be reference clock input (ENET1_REF_CLK1 signal), but above 25MHz clock can be routed to the pin by internal channel of i.MX6SX, so you don't need to connect external clcok to Pad ENET1_TX_CLK.

(2)Connect 15p capacitor between differential lines

One 15pF capacitor between TXP and TXN

One 15pF capacitor between RXP and RXN

   No other issues were found!

Best regards,

Weidong

807 次查看
Richard1z
Contributor II

Hi Weidong.

thank you very much for this helpful information !

R

0 项奖励