RGMII Max Trace Length

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RGMII Max Trace Length

3,027 Views
Balaji_ng
Contributor III

Hi,

    I am designing I.MX6SoloX based PCB with dual AR8031 as in Sabre SDB.  The trace lengths of RGMII on my Layout are approximately 5.6 Inch because of the Placement Constraints. However, all the RGMII traces have an unsplit Ground Reference Plane. As per RGMII standards, I understand maximum RGMII trace length is 6 Inches.

In the above context, let me know if the 5.6 Inch is fine.

Regards,

Balaji.V

Labels (1)
0 Kudos
1 Reply

1,996 Views
igorpadykov
NXP Employee
NXP Employee

Hi Balaji

i.MX does not impose additional restrictions on length, so

5.6 Inch would be fine.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------