RGMII I/O supply mode setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RGMII I/O supply mode setting

455 Views
eishishibusawa
Contributor III

Dear Sir

 

I refer to the IMX6SXIEC Rev. 3.

It has four voltage mode (1.5, 1.8, 2.5 and 3.3V) for RGMII I/O supply.

 

Q1.

Is it necessary to set some register in order to set the voltage mode?

I think that it is only to use within the range of min = 1.43 V, Typ = 1.5 V, max = 1.58 when we want to use it in 1.5V mode.

Is my understanding correct?

Best Regards,

Eishi SHIBUSAWA

Labels (2)
0 Kudos
1 Reply

343 Views
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

>Q1.Is it necessary to set some register in order to set the voltage mode?

no

 

>I think that it is only to use within the range of min = 1.43 V, Typ = 1.5 V, max = 1.58 when we want to use it in >1.5V mode.Is my understanding correct?

yes correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos