RGB666 format in i.Mx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RGB666 format in i.Mx6

4,099 Views
deepanrajanbara
Contributor IV

Hi Sir,

We are currently working on custom board based on i.Mx6 processor and Linux Kernel version 3.10.17.

Our display is LVDS(6 bit) so maximum supported bpp is 18.But when i try to run alph_exe.c which is NXP's ipu test example with the bpp as IPU_PIX_FMT_RGB666 on my board i am getting unimplemented pixel format error.

In order to solve it i found that drivers/video/mxc/mxc_ipuv3_fb.c file need to be modified so i have added the following line in struct mxcfb_pfmt

{IPU_PIX_FMT_RGB666, 18, {12, 6, 0}, { 6, 6, 0}, { 0, 6, 0}, { 0, 0, 0} },

But After adding it also i seem to end up in the same error.and further i checked in NXP community it was mentioned to modify the drivers/mxc/ipu3/ipu_param_mem.h

But for IPU_PIX_FMT_RGB666 what  values need to be added in the ipu_ch_param_init

As now i tried with

case IPU_PIX_FMT_RGB666:

                ipu_ch_param_set_field(&params, 0, 107, 3, 3);  /* bits/pixel */

                ipu_ch_param_set_field(&params, 1, 85, 4, 7);   /* pix format */

                ipu_ch_param_set_field(&params, 1, 78, 7, 31);  /* burst size */

                _ipu_ch_params_set_packing(&params, 6, 0, 6, 6, 6, 12, 8, 18);

                break;

But am not sure this is correct value which i have set.Can anyone help me in setting RGB666 in kernel so that my application works properly.

Is this the change required or is there any other change need to set RGB666 for my framebuffer.

When i checked fbset -fb /dev/fb0

my rgb values point to RGB565 and depth as 16.As per RGB666 the depth should be 18.

Can any one help me to proceed in RGB666.Is it possible or am i doing wrong somwhere.

Thank you,

Deepanraj.A

Labels (4)
0 Kudos
Reply
2 Replies

1,358 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello  Deepanraj A,

It is my understanding that the framebuffer bpp and color format doesn't necessarily need to match the interface bpp and color format. E.g. on i.MX6q sabresd, the default framebuffer is RGB565 and LVDS is RGB666. Would this work for you? Or would you really want to have a RGB666 framebuffer?

Regards,

0 Kudos
Reply

1,358 Views
deepanrajanbara
Contributor IV

Yes I wanted my framebuffer also in RGB666 format

0 Kudos
Reply