Hi,
I am using a RGB interface display of 45 pins which we have connected to the iMX7 sabre board with a adapter since the RGB interface on the sabre is 50 pins. I have set the lcdif device tree to configure the display as below based on the display data sheet. but the display seems to be flipped vertically (mirrored vertically, picture attached). Has anyone faced similar issue? is there any setting in the driver that I am missing that needs to be set for the RGB interface?
&lcdif {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lcdif_dat
&pinctrl_lcdif_ctrl>;
enable-gpio = <&gpio_spi 7 GPIO_ACTIVE_LOW>;
display = <&display0>;
status = "okay";
display0: display {
bits-per-pixel = <24>;
bus-width = <24>;
display-timings {
native-mode = <&timing_wvga>;
/* WVGA Timing*/
timing_wvga: 800x480 {
clock-frequency = <33300000>;
hactive = <800>;
vactive = <480>;
hback-porch = <46>;
hfront-porch = <210>;
vback-porch = <23>;
vfront-porch = <22>;
hsync-len = <20>;
vsync-len = <10>;
de-active = <1>;
hsync-active = <0>;
vsync-active = <0>;
pixelclk-active = <1>;
};
};
};
};
Thanks for your response.
Regards
Arun
Hi Arun,
you can check with the u-boot parameters, while booting time press any key, and type print now see the displayinfo arguments,Like (example"displayinfo Video=mxcfbo ,dev=lcd ,800x480@70,if=RGB565"), set these arguments according to your display,
i hope your display x=800 and y=480 (i.e 800x480 ) then according to this what you got that is correct format only,
if you get any other answer please share it here,
Best Regards
SGN
Hi Arun
one can try to flip image using example in unit tests (imx-test):
..test/pxp_lib_test/pxp_test.c
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
By Default if we have the IMX7 connected to 45 Pin RGB Display, why it should show the image as flipped in attached image. Isn't it a issue with IMX7 RGB Driver or Framebuffer?
As per the question it says the configuration isn't changed other than Device Tree.
By Default, does the RGB Display Driver uses PXP? How can we use the test to fix this concern.
Thanks and Regards,
Yuva