Questions about HW_CLKCTRL_SSPx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about HW_CLKCTRL_SSPx

ソリューションへジャンプ
1,797件の閲覧回数
lategoodbye
Senior Contributor I

Hi,

i've some questions regarding to HW_CLKCTRL_SSPx on the i.MX28, which are not really clear from the reference manual:

What are the exact consequences of changing DIV_FRAC_EN?

Is it necessary to check BUSY or CLKGATE before changing DIV_FRAC_EN?

What does it mean to the DIV field if DIV_FRAC_EN=1?

Is there a relation / constraint between HW_CLKCTRL_SSPx.DIV_FRAC_EN and HW_CLKCTRL_CLKSEQ.BYPASS_SSPx?

Best regards

Stefan Wahren

ラベル(2)
0 件の賞賛
返信
1 解決策
1,548件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Stefan

DIV_FRAC_EN enables fractional divider, this is described in

i.MX28 Reference Manual sect.10.3.2 Fractional Clock Divide Mode

http://cache.freescale.com/files/dsp/doc/ref_manual/MCIMX28RM.pdf

>Is it necessary to check BUSY or CLKGATE before changing DIV_FRAC_EN?

yes

>Is there a relation / constraint between HW_CLKCTRL_SSPx.DIV_FRAC_EN

>and HW_CLKCTRL_CLKSEQ.BYPASS_SSPx?

no, this bit allows to switch to XTAL as clock source for SSP. Please check

description in sect.10.8.26:

"PLL0 and 9-phase fractional divider must already be configured when

this bit is cleared."

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,549件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Stefan

DIV_FRAC_EN enables fractional divider, this is described in

i.MX28 Reference Manual sect.10.3.2 Fractional Clock Divide Mode

http://cache.freescale.com/files/dsp/doc/ref_manual/MCIMX28RM.pdf

>Is it necessary to check BUSY or CLKGATE before changing DIV_FRAC_EN?

yes

>Is there a relation / constraint between HW_CLKCTRL_SSPx.DIV_FRAC_EN

>and HW_CLKCTRL_CLKSEQ.BYPASS_SSPx?

no, this bit allows to switch to XTAL as clock source for SSP. Please check

description in sect.10.8.26:

"PLL0 and 9-phase fractional divider must already be configured when

this bit is cleared."

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信