Question, why F3 of MMPF0100 is recommended for i.MX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, why F3 of MMPF0100 is recommended for i.MX6SL

500 Views
Aemj
Contributor IV

Dear team,

My customer plans to use MMPF0100 for their i.MX6SoloLite board.

In the datasheet of MMPF0100(MMPF0100 Rev.13), Table-1 says that PF0100F1 is used for MCIMX6SLEVK. And the notes of Table-10 says as follows.

“For designs using the i.MX 6SoloLite, it is recommended to use the F3 OTP option instead of the F1 OTP option and F4 OTP option instead of the F2 OTP option.”

The customer needs to know which of F1 or F3 should be used for their design.

Could you explain what the Notes of table-10 mean?

Why is F3 recommended for SoloLite?

Thanks,

Miyamoto

Labels (2)
0 Kudos
3 Replies

425 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

F1,F2 not recommended for use.

Depending what memory is used:

SW3 is used for memory, F3 has 1.2V for LPDDR2, F4 has 1.5V for DDR3

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

425 Views
Aemj
Contributor IV

Hi Igor,

Tanks for your support.

Could you show me why F1 and F3 are not recommended?

Thanks,

Miyamoto

425 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

new parts provide VDDHIGH_IN  powering first, improving

stability of other power voltages during power-up sequence.

VDDHIGH_IN powers control logic of pmic internal power regulators.

Best regards

igor

0 Kudos