Question, i.MX6Q SSI time slot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX6Q SSI time slot

607件の閲覧回数
Aemj
Contributor IV

Hi team,

My customer is facing the issue of unexpected behavior of i.MX6Q SSI.

The customer uses SSI as slave/Network mode. And they want to transfer 4 time-slot data.

As for the register setting, RFEN0, RFEN1 and RDMAE is set to 1.

And only first time slot data is transferred.

Do you have any ideas about the cause of this?

Thanks,

Miyamoto

ラベル(2)
0 件の賞賛
3 返答(返信)

424件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Are you using a Operating system? Or using  the SDK.

After checking the SDK I noticed that it fatures an API to configure the FIFOs. I believe you may find it useful .

https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null&WT_TYPE=Software%...

Best Regards,

Alejandro

0 件の賞賛

424件の閲覧回数
Aemj
Contributor IV

Hi Alejandro,

Thanks for your comment.

Actually, the customer does not use OS. SDK neither.

The customer tried without SDMA and the result was the same.

Only at the first time slot, they saw RDR bit was set and the interruption occurred.

At the 2nd-4th slot, the interruption did not occur.

In the customer’s understanding, the interruption occur at the every time slot.

Is it true?

Thanks,

0 件の賞賛

424件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Sorry for the delay. Yes, the RDR flag is set when the SRX0 is loaded with a new value.

But it is cleared only when the SRX0 is read. I wonder if you can share the code so we can take a look at it.

Best Regards,

Alejandro

0 件の賞賛