Question, i.MX25 maximum ratings for GPIO pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX25 maximum ratings for GPIO pin

598件の閲覧回数
SLICE
Contributor IV

Dear team,

I would like to ask about maximum ratings of i.MX25 GPIO pin.

My customer has a question as following.

In the reference manual of i.MX25(IMX25CEC, Rev.10), ‘input voltage range’ is mentioned as below at Table 5.

Vimax = (-0.5V) to (NVDD + 0.3V)

Is it applicable to GPIO Pins (especially, P4 of pin #)?

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 返信

498件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  Parameter VImax of the table 5 is applicable to for GPIO pins, including

P4, but please pay attention on the CAUTION above the table. In particular,
“Exposure to absolute-maximum-rated conditions for extended periods

may affect device reliability.

Table 5 gives stress ratings only—functional operation of the device is

not implied beyond the conditions indicated in Table 6.”

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信