Hi Community,
We are planning to make a custom board with DCDC_BATT source only configuration which will power-up automatically when the power is supplied.
There are description in the documents of i.MX28 that in case of DCDC_BATT source only configuration, PSWITCH pin must be around MID level for 100ms to power up the IC.
Also, there is a description that "A MID LEVEL PSWITCH state can be generated by connecting the VDDXTAL output of the SoC to PSWITCH through a switch."
I suppose the part "through a switch" is to control power-up manually.
So, is there no problem to connect PSWITCH and VDDXTAL directly to automate power-up?
I could not find the exact same question in the community but if there is one and I just missed it, please redirect me to it.
Thank you in advance,
Hikaru
解決済! 解決策の投稿を見る。
Hi Hikaru
you are right, one can connect VDDXTAL via 1K to PSWITCH.
This triggers the startup automatically.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Hikaru
you are right, one can connect VDDXTAL via 1K to PSWITCH.
This triggers the startup automatically.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------