Hi all
I have a question about Sensor Interface Timings.
Especially, Gated Clock Mode and Non-Gated Clock Mode.
Q1.
Is the data latched at the rising edge of the valid pixel clock ?
In IMX6SDLIEC Rev. 7, 10/2016 , there are following description for Sensor Interface Timing in Gated Clock Mode.
"Data is latched at the rising edge of the valid pixel clocks."
However, it looks the data is latched at falling edge in the Figure 58 of IMX6SDLIEC Rev. 7, 10/2016.
Which is correct ?
Q2.
Is the data latched at the rising edge of the valid pixel clock ?
In IMX6SDLIEC Rev. 7, 10/2016 , there are following description for Sensor Interface Timing in Non-Gated Clock Mode.
"The timing is the same as the gated-clock mode”
However, in the Figure 38-17 and Figure 38-18 of RM, the edge is the oppsite.
Is the data latched at the rising edge of the valid pixel clock in Non-Gated Clock Mode ?
Ko-hey
已解决! 转到解答。
Hi Ko-hey
yes data is latched at the rising edge of pixel clock and
this is valid for Non-Gated Clock Mode too. Please note there is
IPUx_CSI0_SENS_CONF[CSI0_SENS_PIX_CLK_POL] bit which selects the
polarity of pixel clock, described in sect.38.5.151 CSI0 Sensor Configuration Register
(IPUx_CSI0_SENS_CONF) i.MX6SDL Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ko-hey
yes data is latched at the rising edge of pixel clock and
this is valid for Non-Gated Clock Mode too. Please note there is
IPUx_CSI0_SENS_CONF[CSI0_SENS_PIX_CLK_POL] bit which selects the
polarity of pixel clock, described in sect.38.5.151 CSI0 Sensor Configuration Register
(IPUx_CSI0_SENS_CONF) i.MX6SDL Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor
Let me confirm more.
According to the Figure 64, the IPUx_CSIx_DATA is latched at falling edge of IPUx_CSIx_PIX_CLK in Gated clock mode.
However, you answered that data is latched at the rising edge of pixel clock.
So the following figure is wrong. Am I correct ?
If yes, do you have any plan to revise it ?
Ko-hey
Hi Ko-hey
data is latched at the rising edge of pixel clock.
As the polarity of pixel clock can be changed with
IPUx_CSI0_SENS_CONF[CSI0_SENS_PIX_CLK_POL]
so picture above can be consdired as correct too.
Best regards
igor