Question about HW_PINCTRL_EMI_DS_CTRL of i.MX28 (RM 9.4.84)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about HW_PINCTRL_EMI_DS_CTRL of i.MX28 (RM 9.4.84)

Jump to solution
698 Views
hikaruuruno
Contributor III

Hi Community,

I have questions about HW_PINCTRL_EMI_DS_CTRL of i.MX28.

1. Do SLICE0_MA (bit1-0) and SLICE1_MA (bit3-2) set the drive strength of DQM0 and DQM1, too, as well as DQ[00:15],

or the drive strength of DQM is defined by CONTROL_MA (bit11-10)?

2. Which defines the drive strength of DQS/DQSN, DUALPAD_MA or SLICE1/0_MA?

I searched the log of the Community and found a post which mentions that SLICE is related to data, mask, strobe.

https://community.freescale.com/message/479777#479777

But since the description in 9.4.84 of RM shows that the drive strength of DQS/DQSN is set by DUALPAD_MA, I am not sure what SLICE is.

Could anyone please give me the answer to the questions above?

Thank you,

Hikaru Uruno

Labels (1)
Tags (1)
0 Kudos
1 Solution
524 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hikaru

1. yes DQM0 and DQM1 is set by SLICE0_MA

1.jpg

2. DQS/DQSN is set by DUALPAD_MA

2.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
525 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hikaru

1. yes DQM0 and DQM1 is set by SLICE0_MA

1.jpg

2. DQS/DQSN is set by DUALPAD_MA

2.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
524 Views
hikaruuruno
Contributor III

Hi Igor,

Thank you for the answers!

It looks strange that even though Figure 14-7 shows that DQSs are a part of the slices, the drive strength of DQSs is not defined by SLICEx_MA but by DUALPAD_MA...

Best regards,

Hikaru

0 Kudos
524 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hikaru

these are exceptions which are specially mentioned in

DUALPAD_MA description.

Best regards

~igor

0 Kudos