Hi
I have a question about GPIOx_IMR in i.MX6 family.
According to the reference manual, when I want to enable a interrupt function, I set the GPIOx_IMR register to "1".
Generally speaking, "Masked" means the function is ignored.
So when I set the register to "1", the interrupt line is masked and the interrupt function is ignored.
I think if my understanding is correct, the description of the reference manual is wrong.
Which is correct?
If the reference manual is correct, what Will be masked ?
Thank you.
已解决! 转到解答。
Hi ko-hey
you are right: 1 - should be UNMASKED Interrupt n is enabled
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ko-hey
you are right: 1 - should be UNMASKED Interrupt n is enabled
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Igor
Thanks.
I would like to confirm just in case. Following description is correct, isn't it?
0 MASKED — Interrupt n line is disabled. (Default)
1 UNMASKED — Interrupt n line is enabled.
Ko-hey