QWKS-SCMIMX6 - write micro sd card with MFG Tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QWKS-SCMIMX6 - write micro sd card with MFG Tools

1,045 Views
pupospace
Contributor I

I'm developing my embedded board with SCM-IMX6Q.
I bought 2 QWKS-SCMIMX6, 1 rev B and 1 rev C.
My embedded board is equipped with Yocto Linus on an eMMC.
I tried download from NXP site SCM-i.MX 6 Series Manufacturing Toolkit for Linux 4.1.15_2.0.0 Release, I set the switch to run in mfg tool mode, I launched the correct file to update with OS image to micro SD Card (mfgtool2-yocto-mx6dqscm-1gb-qwks-rev2-sd.vbs for rev B rev 3 for rev C).
When the mfg tool copy rootfs every time
/ linuxrc: line 14: 73 SegmentaKernel panic - not syncing: Attempted to kill init! ExitCode = 0x00008b00

I tried copy a small rootfs (few MB) and it works, when I tried 10 or more MB, the copy not work.
I tried recompile mfg tool source with last version and not work.
i tried download Android version SCM_IMX6_M6.0.1_2.1.0_MFGTOOL from site and missing 1 file, I found this file in Yocto Linux version, and not work, the issue is the same.

The issue is on both evaluation board, I tried run mfg tool on win xp, win 7 and win 10, and I tried change sd card size and manufacter with the same result.

Anyone can help me?
If I product my embedded board with eMMC, how can I send image if mfg tools not work correctly?

I attach serial debug

U-Boot 2015.04-00323-gd094c3d-dirty (Feb 17 2016 - 16:11:16)

CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 36 C
Reset cause: POR
Board: MX6DQSCM-QWKS
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1 is current device
Net: Phy 3 not found
PHY reset timed out
FEC [PRIME]
Error: FEC address not set.

Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Kernel image @ 0x12000000 [ 0x000000 - 0x552a48 ]
## Loading init Ramdisk from Legacy Image at 12c00000 ...
Image Name: fsl-image-mfgtool-initramfs-imx6
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 7565864 Bytes = 7.2 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Using Device Tree in place at 18000000, end 1800c1b1

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 4.1.15-1.0.0-mfgtool+g3924425 (bamboo@shlinux12) (gcc version 5.2.0 (GCC) ) #1 SMP PREEMPT Sun Mar 13 17:19:17 CST 2016
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6DQ SCM QWKS
Reserved memory: created CMA memory pool at 0x1c000000, size 320 MiB
Reserved memory: initialized node linux,cma, compatible id shared-dma-pool
Memory policy: Data cache writealloc
PERCPU: Embedded 12 pages/cpu @8ad05000 s16768 r8192 d24192 u49152
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 261120
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= enable_wait_mode=off
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 693416K/1048576K available (6895K kernel code, 319K rwdata, 2412K rodata, 388K init, 423K bss, 27480K reserved, 327680K cma-reserved, 524288K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xa0800000 - 0xff000000 (1512 MB)
lowmem : 0x80000000 - 0xa0000000 ( 512 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x8091ef88 (9308 kB)
.init : 0x8091f000 - 0x80980000 ( 388 kB)
.data : 0x80980000 - 0x809cff00 ( 320 kB)
.bss : 0x809d2000 - 0x80a3bf14 ( 424 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Preemptible hierarchical RCU implementation.
Additional per-CPU info printed with stalls.
NR_IRQS:16 nr_irqs:16 16
L2C-310 erratum 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 16 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 16 ways, 1024 kB
L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76070001
mxc_clocksource_init 3000000
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x10008280 - 0x100082f0
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
Brought up 4 CPUs
SMP: Total of 4 processors activated (24.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
CPU identified as i.MX6Q, silicon rev 1.5
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
mxs-dma 110000.dma-apbh: initialized
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA
i2c i2c-2: IMX I2C adapter registered
i2c i2c-2: can't use DMA
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 7392K (82c00000 - 83338000)
CPU PMU: Failed to parse /soc/pmu/interrupt-affinity[0]
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 1024 (order: 4, 65536 bytes)
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.23)
bounce: pool size: 64 pages
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight supply power not found, using dummy regulator
mxc_sdc_fb fb@0: NO mxc display driver found!
mxc_sdc_fb fb@1: NO mxc display driver found!
mxc_sdc_fb fb@2: NO mxc display driver found!
mxc_sdc_fb fb@3: NO mxc display driver found!
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.3
imx-sdma 20ec000.sdma: initialized
pfuze100-regulator 1-0008: Full layer: 2, Metal layer: 1
pfuze100-regulator 1-0008: FAB: 0, FIN: 0
pfuze100-regulator 1-0008: pfuze100 found.
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 24, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
m25p80 spi0.0: n25q128a13 (16384 Kbytes)
spi_imx 2008000.ecspi: probed
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
LUN: removable file: (no medium)
Number of LUNs=1
Number of LUNs=1
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
mousedev: PS/2 mouse device common for all mice
egalax_ts 1-0004: Failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
egalax_ts 2-0004: Failed to read firmware version
egalax_ts: probe of 2-0004 failed with error -5
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified
sdhci-esdhc-imx 2194000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2194000.usdhc: Got WP GPIO
sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
/soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified
sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2198000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mxc_vpu 2040000.vpu_fsl: VPU initialized
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
Key type dns_resolver registered
mmc2: host does not support reading read-only switch, assuming write-enable
mmc2: new high speed SDHC card at address 59b4
mmcblk2: mmc2:59b4 EB2MW 29.8 GiB
mmcblk2: p1 p2
Registering SWP/SWPB emulation handler
input: gpio-keys as /devices/soc0/gpio-keys/input/input2
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
usb_otg_vbus: disabling
ALSA device list:
No soundcards found.
Freeing unused kernel memory: 388K (8091f000 - 80980000)
Starting UTP
uuc 0.5 [built Mar 12 2016 19:04:20]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ tar xf $FILE '
UTP: executing "tar xf $FILE "
UTP: sending Success to kernel for command $ tar xf $FILE .
utp_poll: pass returned.
UTP: received command '$ sh mksdcard.sh /dev/mmcblk2'
UTP: executing "sh mksdcard.sh /dev/mmcblk2"
1+0 records in
1+0 records out
1024 bytes (1.0 kB) copied, 0.113665 s, 9.0 kB/s
Checking that no-one is using thirandom: sfdisk urandom read with 9 bits of entropy available
s disk right now ... OK

Disk /dev/mmcblk2: 29.8 GiB, 32026656768 bytes, 62552064 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes

>>> Created a new DOS disklabel with disk identifier 0xbe9bfd4b.
Created a new partition 1 of type 'W95 FAT32 (LBA)' and of size 500 MiB.
/dev/mmcblk2p2: Created a new partition 2 of type 'Linux' and of size 29.2 GiB.
/dev/mmcblk2p3:
New situation:

Device Boot Start End Sectors Size Id Type
/dev/mmcblk2p1 20480 1044479 1024000 500M c W95 FAT32 (LBA)
/dev/mmcblk2p2 1228800 62552063 61323264 29.2G 83 Linux

The partition table has been altered.
Calling ioctl() to re-read partit mmcblk2: p1 p2
ion table.
Syncing disks.
UTP: sending Success to kernel for command $ sh mksdcard.sh /dev/mmcblk2.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ dd if=/dev/zero of=/dev/mmcblk2 bs=1k seek=768 conv=fsync count=129'
UTP: executing "dd if=/dev/zero of=/dev/mmcblk2 bs=1k seek=768 conv=fsync count=129"
129+0 records in
129+0 records out
132096 bytes (132 kB) copied, 0.564457 s, 234 kB/s
UTP: sending Success to kernel for command $ dd if=/dev/zero of=/dev/mmcblk2 bs=1k seek=768 conv=fsync count=129.
utp_poll: pass returned.
UTP: received command '$ dd if=$FILE of=/dev/mmcblk2 bs=1k seek=1 conv=fsync'
UTP: executing "dd if=$FILE of=/dev/mmcblk2 bs=1k seek=1 conv=fsync"
467+0 records in
467+0 records out
478208 bytes (478 kB) copied, 1.54736 s, 309 kB/s
UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk2 bs=1k seek=1 conv=fsync.
utp_poll: pass returned.
UTP: received command '$ while [ ! -e /dev/mmcblk2p1 ]; do sleep 1; echo "waiting..."; done '
UTP: executing "while [ ! -e /dev/mmcblk2p1 ]; do sleep 1; echo "waiting..."; done "
UTP: sending Success to kernel for command $ while [ ! -e /dev/mmcblk2p1 ]; do sleep 1; echo "waiting..."; done .
utp_poll: pass returned.
UTP: received command '$ mkfs.vfat /dev/mmcblk2p1'
UTP: executing "mkfs.vfat /dev/mmcblk2p1"
mkfs.fat 3.0.28 (2015-05-16)
UTP: sending Success to kernel for command $ mkfs.vfat /dev/mmcblk2p1.
utp_poll: pass returned.
UTP: received command '$ mkdir -p /mnt/mmcblk2p1'
UTP: executing "mkdir -p /mnt/mmcblk2p1"
UTP: sending Success to kernel for command $ mkdir -p /mnt/mmcblk2p1.
utp_poll: pass returned.
UTP: received command '$ mount -t vfat /dev/mmcblk2p1 /mnt/mmcblk2p1'
UTP: executing "mount -t vfat /dev/mmcblk2p1 /mnt/mmcblk2p1"
UTP: sending Success to kernel for command $ mount -t vfat /dev/mmcblk2p1 /mnt/mmcblk2p1.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ cp $FILE /mnt/mmcblk2p1/zImage'
UTP: executing "cp $FILE /mnt/mmcblk2p1/zImage"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk2p1/zImage.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ cp $FILE /mnt/mmcblk2p1/imx6dqscm-1gb-qwks-rev2-fix-ldo.dtb'
UTP: executing "cp $FILE /mnt/mmcblk2p1/imx6dqscm-1gb-qwks-rev2-fix-ldo.dtb"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk2p1/imx6dqscm-1gb-qwks-rev2-fix-ldo.dtb.
utp_poll: pass returned.
UTP: received command '$ cp $FILE /mnt/mmcblk2p1/imx6dqscm-1gb-qwks-rev2-fix-ldo.dtb'
UTP: executing "cp $FILE /mnt/mmcblk2p1/imx6dqscm-1gb-qwks-rev2-fix-ldo.dtb"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk2p1/imx6dqscm-1gb-qwks-rev2-fix-ldo.dtb.
utp_poll: pass returned.
UTP: received command '$ umount /mnt/mmcblk2p1'
UTP: executing "umount /mnt/mmcblk2p1"
UTP: sending Success to kernel for command $ umount /mnt/mmcblk2p1.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext3 -j /dev/mmcblk2p2'
UTP: executing "mkfs.ext3 -j /dev/mmcblk2p2"
mke2fs 1.42.9 (28-Dec-2013)
random: nonblocking pool is initialized
Discarding device blocks: done
Filesystem label=
OS type: Linux
Block size=4096 (log=2)
Fragment size=4096 (log=2)
Stride=0 blocks, Stripe width=0 blocks
1916928 inodes, 7665408 blocks
383270 blocks (5.00%) reserved for the super user
First data block=0
Maximum filesystem blocks=0
234 block groups
32768 blocks per group, 32768 fragments per group
8192 inodes per group
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632, 2654208,
4096000

Allocating group tables: done
Writing inode tables: done
Creating journal (32768 blocks): done
Writing superblocks and filesystem accounting information: done

UTP: sending Success to kernel for command $ mkfs.ext3 -j /dev/mmcblk2p2.
utp_poll: pass returned.
UTP: received command '$ mkdir -p /mnt/mmcblk2p2'
UTP: executing "mkdir -p /mnt/mmcblk2p2"
UTP: sending Success to kernel for command $ mkdir -p /mnt/mmcblk2p2.
utp_poll: pass returned.
UTP: received command '$ mount -t ext3 /dev/mmcblk2p2 /mnt/mmcblk2p2'
UTP: executing "mount -t ext3 /dev/mmcblk2p2 /mnt/mmcblk2p2"
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk2p2): using internal journal
EXT3-fs (mmcblk2p2): mounted filesystem with ordered data mode
UTP: sending Success to kernel for command $ mount -t ext3 /dev/mmcblk2p2 /mnt/mmcblk2p2.
utp_poll: pass returned.
UTP: received command 'pipe tar -jxv -C /mnt/mmcblk2p2'
pid is 96, UTP: executing "tar -jxv -C /mnt/mmcblk2p2"
UTP: sending Success to kernel for command pipe tar -jxv -C /mnt/mmcblk2p2.
./
./dev/
./var/
./var/run
./var/volatile/
./var/backups/
./var/local/
./var/spool/
./var/spool/at/
./var/spool/at/spool/
./var/spool/at/jobs/
./var/spool/at/jobs/.SEQ
./var/spool/mail/
./var/spool/cron/
./var/spool/cron/root
./var/cache/
./var/cache/ldconfig/
./var/cache/ldconfig/aux-cache
./var/cache/fontconfig/
./var/cache/fontconfig/CACHEDIR.TAG
./var/cache/fontconfig/94322f4d3cdf1bd54794b691285ca062-le32d8.cache-6
./var/cache/fontconfig/6ba42ae0000f58711b5caaf10d690066-le32d8.cache-6
./var/cache/fontconfig/3830d5c3ddfd5cd38a049b759396e72e-le32d8.cache-6
./var/log
./var/lock
./var/lib/
./var/lib/dbus/
./var/lib/alsa/
./var/lib/alsa/asound.state
./var/lib/logrotate.status
./var/lib/misc/
./var/lib/sudo/
./var/lib/sudo/lectured/
./var/lib/nfs/
./var/lib/nfs/rmtab
./var/lib/nfs/xtab
./var/lib/nfs/v4recovery/
./var/lib/nfs/statd/
./var/lib/nfs/statd/sm/
./var/lib/nfs/statd/sm.bak/
./var/lib/nfs/statd/state
./var/lib/nfs/etab
./var/lib/arpd/
./var/lib/urandom/
./var/tmp
./boot/
./boot/zImage-4.1.15-2.0.0+g7a75e7f
./boot/zImage
./run/
./usr/
./usr/games/
./usr/games/inertia
./usr/games/slant
./usr/games/map
./usr/games/fifteen
./usr/games/bridges
./usr/games/samegame
./usr/sbin/
./usr/sbin/hostap_io_debug
./usr/sbin/nl-cls-delete
./usr/sbin/rpcinfo
./usr/sbin/start-statd
./usr/sbin/chcpu
./usr/sbin/flash_otp_info
./usr/sbin/resizepart
./usr/sbin/exportfs
./usr/sbin/adduser
./usr/sbin/v4l2-dbg
./usr/sbin/powertop
./usr/sbin/gensprep
./usr/sbin/iw
./usr/sbin/gencmn
./usr/sbin/nl-class-list
./usr/sbin/addpart
./usr/sbin/update-rc.d
./usr/sbin/mkfs
./usr/sbin/pwck
./usr/sbin/xtables-multi
./usr/sbin/pwunconv
./usr/sbin/sm-notify
./usr/sbin/blktool
./usr/sbin/nl-classid-lookup
./usr/sbin/ubiupdatevol
./usr/sbin/fbset
./usr/sbin/zcav
./usr/sbin/ip6tables-save
./usr/sbin/rpcbind
./usr/sbin/ldattach
./usr/sbin/udhcpd
./usr/sbin/cracklib-format
./usr/sbin/fdformat
./usr/sbin/chpasswd.shadow
./usr/sbin/hostap_fw_load
./usr/sbin/nandwrite
./usr/sbin/update-pciids
./usr/sbin/rpc.idmapd
./usr/sbin/hostap_diag
./usr/sbin/wpa_supplicant
./usr/sbin/crond
./usr/sbin/hostap_rid
./usr/sbin/nl-qdisc-delete
./usr/sbin/nologin
./usr/sbin/loadfont
./usr/sbin/nl-cls-list
./usr/sbin/ubinize
./usr/sbin/connmand
/linuxrc: line 14: 73 SegmentaKernel panic - not syncing: Attempted to kill init! exitcode=0x00008b00

Pion fault uucC
U3: stopping
CPU: 3 PID: 97 Comm: tar Not tainted 4.1.15-1.0.0-mfgtool+g3924425 #1
Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[<80015ee4>] (unwind_backtrace) from [<80012774>] (show_stack+0x10/0x14)
[<80012774>] (show_stack) from [<8068fca4>] (dump_stack+0x80/0xc8)
[<8068fca4>] (dump_stack) from [<80014d14>] (handle_IPI+0x15c/0x190)
[<80014d14>] (handle_IPI) from [<80009478>] (gic_handle_irq+0x58/0x60)
[<80009478>] (gic_handle_irq) from [<80013524>] (__irq_usr+0x44/0x60)
Exception stack(0x880fffb0 to 0x880ffff8)
ffa0: 000000eb 000000e5 0000350c 0000000e
ffc0: 0002ef0e 0152ddec 00000000 0152dde8 015250f1 01524098 76a17008 ffffffff
ffe0: 7e89c6c8 7e89c530 000057ff 00056008 20060010 ffffffff
CPU1: stopping
CPU: 1 PID: 0 Comm: swapper/1 Not tainted 4.1.15-1.0.0-mfgtool+g3924425 #1
Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[<80015ee4>] (unwind_backtrace) from [<80012774>] (show_stack+0x10/0x14)
[<80012774>] (show_stack) from [<8068fca4>] (dump_stack+0x80/0xc8)
[<8068fca4>] (dump_stack) from [<80014d14>] (handle_IPI+0x15c/0x190)
[<80014d14>] (handle_IPI) from [<80009478>] (gic_handle_irq+0x58/0x60)
[<80009478>] (gic_handle_irq) from [<80013240>] (__irq_svc+0x40/0x74)
Exception stack(0x8608df60 to 0x8608dfa8)
df60: 00000000 8ad172c0 00000001 8608c000 0c6841e1 00000043 0cde22f6 00000043
df80: 8ad13dd8 00000001 8097a304 00000001 ffffffff 8608dfa8 806953a4 804a861c
dfa0: 20060013 ffffffff
[<80013240>] (__irq_svc) from [<804a861c>] (cpuidle_enter_state+0xcc/0x1f8)
[<804a861c>] (cpuidle_enter_state) from [<800657c0>] (cpu_startup_entry+0x1d0/0x314)
[<800657c0>] (cpu_startup_entry) from [<1000950c>] (0x1000950c)
CPU0: stopping
CPU: 0 PID: 0 Comm: swapper/0 Not tainted 4.1.15-1.0.0-mfgtool+g3924425 #1
Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[<80015ee4>] (unwind_backtrace) from [<80012774>] (show_stack+0x10/0x14)
[<80012774>] (show_stack) from [<8068fca4>] (dump_stack+0x80/0xc8)
[<8068fca4>] (dump_stack) from [<80014d14>] (handle_IPI+0x15c/0x190)
[<80014d14>] (handle_IPI) from [<80009478>] (gic_handle_irq+0x58/0x60)
[<80009478>] (gic_handle_irq) from [<80013240>] (__irq_svc+0x40/0x74)
Exception stack(0x80981f28 to 0x80981f70)
1f20: 00000000 8ad0b2c0 00000001 80980000 0c6875f6 00000043
1f40: 0cde0a39 00000043 8ad07dd8 00000001 8097a304 00000001 ffffffff 80981f70
1f60: 806953a4 804a861c 20070113 ffffffff
[<80013240>] (__irq_svc) from [<804a861c>] (cpuidle_enter_state+0xcc/0x1f8)
[<804a861c>] (cpuidle_enter_state) from [<800657c0>] (cpu_startup_entry+0x1d0/0x314)
[<800657c0>] (cpu_startup_entry) from [<8091fbfc>] (start_kernel+0x334/0x3a0)
---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x00008b00

Labels (2)
0 Kudos
1 Reply

522 Views
igorpadykov
NXP Employee
NXP Employee

Hi pupospace

for programming sd one can follow sect.4.3 Preparing an SD/MMC card to boot Linux Guide

included in Documentation:

https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS 

Pay attention to sect.4.3.3 Partitioning the SD/MMC card (corresponds to mfg tools script

../OS Firmware/mksdcard.sh.tar) and SCM Demo images:

Board Support Packages (3)
Demo Images - QWKS Board based on SCM-i.MX 6D/Q(REV C)

Quick Start Board for SCM-i.MX 6DQ|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos