Q10.0.0_2.3.0_ANDROID_SOURCE works on MCIMX8QXP-CPU does not support ADB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Q10.0.0_2.3.0_ANDROID_SOURCE works on MCIMX8QXP-CPU does not support ADB

Jump to solution
1,401 Views
relax-wu
Contributor IV

i flash Q10.0.0_2.3.0_DEMO_8Q img to MCIMX8QXP-CPU,but I can't connect to it using adb.

I compile the image generated by Q10.0.0_2.3.0_ANDROID_SOURCE and it will not work.

Do I need to modify anything?

 

 

0 Kudos
1 Solution
1,251 Views
relax-wu
Contributor IV

I don't know, I didn't pay attention, I directly started to configure mipi display, and then adb was fine.

Before comparison, i2c-adapter has increased a lot,Looks like M4 started。

mek_8q:/ # i2cdetect -l
i2c-1   i2c             i2c-rpmsg-adapter                       I2C Adapter
i2c-17  i2c             56226000.i2c                            I2C Adapter
i2c-15  i2c             i2c-rpmsg-adapter                       I2C Adapter
i2c-18  i2c             56246000.i2c                            I2C Adapter
i2c-16  i2c             58226000.i2c                            I2C Adapter
i2c-14  i2c             i2c-rpmsg-adapter                       I2C Adapter
i2c-5   i2c             i2c-rpmsg-adapter                       I2C Adapter
i2c-12  i2c             i2c-rpmsg-adapter                       I2C Adapter
 
 

View solution in original post

10 Replies
1,353 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Have you install the Android SDK Platform-Tools?

https://developer.android.com/studio/command-line/adb

0 Kudos
1,348 Views
relax-wu
Contributor IV

I have installed adb tool。If I use Q10.0.0_2.2.0_AUTO_DEMO_8Q, I can connect to it using adb

0 Kudos
1,363 Views
relax-wu
Contributor IV

Q10.0.0_2.5.0_DEMO_8Q also failed!

0 Kudos
1,354 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

What's your steps?

0 Kudos
1,351 Views
relax-wu
Contributor IV

https://www.nxp.com.cn/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-8quadxp...  

download Q10.0.0_2.3.0_DEMO_8Q ,and Execute .\uuu_imx_android_flash.bat -f imx8qxp。

Boot machine, I cannot use adb to connect to the machine on the computer, and neither of the two usb ports will work.

 

0 Kudos
1,342 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version MCIMX8QXP-CPU board are you using, B0 or C0  version?

0 Kudos
1,301 Views
relax-wu
Contributor IV

Good morning, is there a result?

0 Kudos
1,338 Views
relax-wu
Contributor IV

I am using the official development kit. B0 version

0 Kudos
1,254 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Does it work well on your side? In my board I install the Android SDK Platform-Tools will be OK.

0 Kudos
1,252 Views
relax-wu
Contributor IV

I don't know, I didn't pay attention, I directly started to configure mipi display, and then adb was fine.

Before comparison, i2c-adapter has increased a lot,Looks like M4 started。

mek_8q:/ # i2cdetect -l
i2c-1   i2c             i2c-rpmsg-adapter                       I2C Adapter
i2c-17  i2c             56226000.i2c                            I2C Adapter
i2c-15  i2c             i2c-rpmsg-adapter                       I2C Adapter
i2c-18  i2c             56246000.i2c                            I2C Adapter
i2c-16  i2c             58226000.i2c                            I2C Adapter
i2c-14  i2c             i2c-rpmsg-adapter                       I2C Adapter
i2c-5   i2c             i2c-rpmsg-adapter                       I2C Adapter
i2c-12  i2c             i2c-rpmsg-adapter                       I2C Adapter